This is an old revision of the document!
The ADuCM360_demo_cn0396 is a dual toxic gas detector demo project, for the EVAL-ADICUP360 base board with additional EVAL-CN0396-ARDZ shield, created using the GNU ARM Eclipse Plug-ins in Eclipse environment.
The ADuCM360_demo_cn0396 project uses the EVAL-CN0396-ARDZ shield which is a single-supply, low noise, portable gas detector, using a 4-electrode electrochemical sensor, for simultaneous detection of two distinct gases - for this example is used the Alphasense COH-A2 sensor, which detects carbon monoxide(CO) and hydrogen sulfide(H2S).
The EVAL-CN0396-ARDZ board provides a potentiostatic circuit for biasing the electrochemical sensor, along with dual programmable TIA's and 16-bit Sigma-Delta ADC. The TIA's convert the small currents passing in the sensor to a voltage that can be read by the AD7798 a 3-channel, low noise, low power 16-bit ADC that converts the analog voltage into digital data. The 16-bit ADC outputs are received via SPI interface of the EVAL-ADICUP360 board. An ADT7310 digital temperature sensor is also included to measure ambient temperature in order for correction of temperature effects.
The ADuCM360_demo_cn0396 application reads temperature value from ADT7310 and ADC values for each gas channel (CO and H2S), processes the values and make all necessary conversions in order to provide the gas concentrations. A UART interface (115200 baud rate and 8-bits data length) is used to send the results to terminal window. The output data will be displayed continuously considering a data refresh parameter (see DISPLAY_REFRESH).
Based on the maximum sensor sensitivity for each gas the system should be configured before using it. The application will calculate the gas concentration using sensor gas sensitivity and then compensate these values using measured temperature value.
Connect the EVAL-CN0396-ARDZ to the Arduino connectors P4, P5, P6, P7, P8 of the EVAL-ADICUP360 board.
In order to program the base board you need to use the DEBUG USB, and you will need to use the USER USB to communicate with the serial terminal program. The important jumpers and switches configurations are highlighted in red.
The ADuCM360_demo_cn0396 uses UART connection via P0.6/P0.7 and SPI1 channel of the ADuCM360 to communicate with EVAL-CN0396-ARDZ board. The CS1 for AD7798 is configured on P0.3, the CS2 for AD5270 is configured on P1.4 and the CS3 for ADT7310 on P1.2. See jumper setup in the picture below:
We recommend not opening the project directly, but rather import it into Eclipse and make a local copy in your Eclipse workspace.
The source code and include files of the ADuCM360_demo_cn0396 can be found on Github:
The necessary instructions on how to import the ADuCM360_demo_cn0396 project form the projects examples in the Git repository, can be found in How to import existing projects from the GIT Repository page.
After completion of the steps above the program will remain written into the system flash and it will run by default every time the board is powered up.
The ADuCM360_demo_cn0396 is a C project which uses ADuCM36x C/C++ Project structure.
This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripherals; port configuration for SPI1, UART via P0.6/P0.7; SPI, UART read/write functions, AD7798 control, AD5270 and ADT7310 control; gas concentration computation.
In the src and include folders you will find the source and header files related to CN0396 software application. The Communication.c/h files contain SPI and UART specific data, the AD7798.c/h files contain the ADC control, the AD5270.c/h files contain the rheostat control, the ADT73100.c/h files contain the temperature sensor control, and the CN0396.c/h files are for the gas calculations.
In the appropriate header files you can configure next parameters:
#define CO_RANGE 1000 #define H2S_RANGE 200
#define CO_SENS (75 * pow(10, -9)) #define H2S_SENS (800 * pow(10, -9))
#define MAX_CO_SENS (100 * pow(10, -9)) #define MAX_H2S_SENS (1000 * pow(10, -9))
* Terminal refresh - DISPLAY_REFRESH parameter - how often to refresh the output data - input time value in [msec] (CN0396.h).
#define DISPLAY_REFRESH 500
The system folder contains system related files (try not to change these files):