This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0391 [03 Jan 2021 21:46] – fix links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0391 [04 Jan 2021 21:56] – Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Multichannel Thermocouple - Digital Outputs - Demo ====== | ====== Multichannel Thermocouple - Digital Outputs - Demo ====== | ||
- | The **ADuCM360_demo_cn0391** is a temperature measurement demo project which uses the thermocouple principle of measurement with the EVAL-ADICUP360 base board and an additional [[adi>en/ | + | The **ADuCM360_demo_cn0391** is a temperature measurement demo project which uses the thermocouple principle of measurement with the EVAL-ADICUP360 base board and an additional [[adi> |
===== General description ===== | ===== General description ===== | ||
- | The **ADuCM360_demo_cn0391** project uses the [[adi>en/ | + | The **ADuCM360_demo_cn0391** project uses the [[adi> |
- | The EVAL-CN0391-ARDZ shield uses the [[adi>en/ | + | The EVAL-CN0391-ARDZ shield uses the [[adi>AD7124-8|AD7124-8 part]] which is a **8-Channel** Low Noise, Low Power, **24-Bit**, Sigma-Delta **ADC** with PGA and Reference. All signal conditioning and excitation is performed by the AD7124-8, no additional components are needed. |
{{: | {{: | ||
Line 45: | Line 45: | ||
\\ | \\ | ||
- | < | ||
- | The second approximation formula was implemented for [[adi> | ||
- | </ | ||
==== Thermocouple Measurement ==== | ==== Thermocouple Measurement ==== |