This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0357_ism43340 [16 Sep 2016 15:34] – Manali Vispute | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0357_ism43340 [16 Sep 2016 15:57] (current) – Manali Vispute | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== General Description ===== | ===== General Description ===== | ||
- | This project is a good example of how to use the EVAL-ADICUP360 board and Inventek System' | + | This project is a good example of how to use the EVAL-ADICUP360 board and Inventek System' |
The ISMART is an Arduino compatible shield, that consists of an Inventek eS-WiFi module ISM43340 which leverages Broadcom' | The ISMART is an Arduino compatible shield, that consists of an Inventek eS-WiFi module ISM43340 which leverages Broadcom' | ||
Line 17: | Line 17: | ||
| | ||
| | ||
- | The EVAL-CN0357-ARDZ shield circuit provides a potentiostatic circuit for biasing the electrochemical sensor, along with a programmable TIA and 16-bit Sigma-Delta ADC. The TIA converts the small currents passing in the sensor to a voltage that can be read by the ADC. The 16-bit ADC value is received via SPI interface of the EVAL-ADICUP360 board, where the gas concentration is computed. The ADuCM360_ISM43340_CN0357 application configures the necessary components, processes ADC output value and make all necessary conversions in order to provide the gas concentration in Parts Per Million (PPM). | + | The EVAL-CN0357-ARDZ shield circuit provides a potentiostatic circuit for biasing the electrochemical sensor, along with a programmable TIA and 16-bit Sigma-Delta ADC. The TIA converts the small currents passing in the sensor to a voltage that can be read by the ADC. The 16-bit ADC value is received via SPI interface of the EVAL-ADICUP360 board, where the gas concentration is computed. The ADuCM360_ISM43340_CN0357 application configures the necessary components, processes ADC output value and make all necessary conversions in order to provide the gas concentration in Parts Per Million (PPM). |
At the start of the project, the software computes the necessary parameters and configures the digital rheostat(AD5270) of the TIA. The required parameters are the sensor sensitivity and sensor range. These can be modified by changing the values of the constants SENSOR_SENSITIVITY and SENSOR_RANGE found in the CN0357.h header file of the project. See the “Project Structure” section for more details. | At the start of the project, the software computes the necessary parameters and configures the digital rheostat(AD5270) of the TIA. The required parameters are the sensor sensitivity and sensor range. These can be modified by changing the values of the constants SENSOR_SENSITIVITY and SENSOR_RANGE found in the CN0357.h header file of the project. See the “Project Structure” section for more details. | ||
Line 98: | Line 98: | ||
</ | </ | ||
- | * **ssid** - <fc # | + | * **WLAN SSID** - <fc # |
< | < | ||
char ssid[] = "< Enter WLAN SSID >" | char ssid[] = "< Enter WLAN SSID >" | ||
</ | </ | ||
- | * **password** - <fc # | + | * **WLAN Password** - <fc # |
< | < | ||
- | char ssid[] = "< Enter WLAN Password >" | + | char password[] = "< Enter WLAN Password >" |
</ | </ | ||
- | * **security_type** - <fc # | + | * **WLAN Security Type** - <fc # |
< | < | ||
- | char ssid[] = "< Enter WLAN Security Type >" | + | char security_type[] = "< Enter WLAN Security Type >" |
</ | </ | ||
- | * **Thing_Name** - <fc # | + | * **Thing Name** - <fc # |
char Thing_Name[] = "< Enter Thing Name >" | char Thing_Name[] = "< Enter Thing Name >" | ||
</ | </ | ||
- | * **Application Key** - <fc #008000>Application Key</fc> - Application Key associated with user account(// | + | * **Application Key** - <fc #008000>app_key</fc> - Application Key associated with user account(// |
< | < | ||
char app_key[] = "< Enter Application Key >" | char app_key[] = "< Enter Application Key >" | ||
</ | </ | ||
\\ | \\ | ||
- | |||
The **system** folder contains system related files (try not to change these files): | The **system** folder contains system related files (try not to change these files): | ||
* **ADuCM360** – contains low levels drivers for ADuCM360 microcontroller. | * **ADuCM360** – contains low levels drivers for ADuCM360 microcontroller. |