This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cli [14 Jan 2021 05:23] – use / interwiki links Robin Getz | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cli [14 Mar 2021 06:15] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 79: | Line 79: | ||
\\ | \\ | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | \\ | + | |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging and Dropping the .Bin to the MBED drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. | ||
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_cli** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
+ | Prebuilt CLI Demo Bin File | ||
+ | * [[https:// | ||
+ | Complete CLI Demo Source Files | ||
+ | * [[https:// | ||
- | [[https:// | ||
- | |||
</ | </ | ||