This is an old revision of the document!
The ADuCM360_demo_blink is the simplest possible demo project for the EVAL-ADICUP360, created using the GNU ARM Eclipse Plug-ins in Eclipse environment.
The project includes basic initialization - stopping the watchdog, configuring the system clock, disabling the clocks for all peripherals and setting two digital outputs for driving the two LEDs on the board: LED2 and LED3. The automatically generated code by the GNU ARM Eclipse Plug-ins provide a system tick interrupt at 1ms intervals and a simple delay function.
This project uses the low level drivers available for ADuCM360 microcontroller. It provide the possibility to choose the LEDs blinking method: use the delay function or use timer interrupt service.
When the project is compiled and run, the two LEDs flash alternatively in predefined intervals (1 second for delay function method and 0.5 seconds for timer interrupt method).
We recommend not opening the project directly, but rather import it into Eclipse and make a local copy in your Eclipse workspace.
To learn how to import the ADuCM360_demo_blink project from the projects examples in the Git repository, please click on How to import existing projects from the GIT Repository.
The source code and include files for the ADuCM360_demo_blink can be found in projects examples which comes with installer package, or the latest version of the project can be found on Github:
The necessary instructions on how to import ADuCM360_demo_blink project in your workspace can be found in the section, Import a project into workspace.
After completion of the steps above the program will remain written into the system flash and it will run by default every time the board is powered up.
The ADuCM360_demo_blink project use basic ARM Cortex-M C/C++ Project structure:
In the src and include folders you will find the source and header files related to blink application. You can modify as you wanted those files.
Here you can configure:
The system folder contains system related files (try not to change these files):