This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [03 Jan 2017 18:31] – added configurable variable in the c code Brandon Bushey | resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [14 Mar 2021 06:08] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADT7420 PMOD Temperature Demo ====== | ====== ADT7420 PMOD Temperature Demo ====== | ||
- | The **ADuCM360_demo_adt7420_pmdz** is a temperature demo project for the EVAL-ADICUP360 base board with an EVAL_ADT7420-PMDZ PMOD board from Analog Devices, using the GNU ARM Eclipse Plug-ins in Eclipse environment. | + | The **ADuCM360_demo_adt7420_pmdz** is a temperature demo project for the EVAL-ADICUP360 base board with an EVAL-ADT7420-PMDZ PMOD board from Analog Devices, using the GNU ARM Eclipse Plug-ins in Eclipse environment. |
===== General description ===== | ===== General description ===== | ||
- | This project is an example for how to use [[resources: | + | This project is an example for how to use [[resources: |
The ADuCM360_demo_adt7420_pmdz project uses the [[ADI> | The ADuCM360_demo_adt7420_pmdz project uses the [[ADI> | ||
Line 11: | Line 11: | ||
{{ : | {{ : | ||
- | The application reads the temperature data from the ADT7420 and displays the temperature in **[codes]** and **[C]** on a serial terminal. | + | The application reads the temperature data from the ADT7420 and displays the temperature in **[codes]** and **[C]** on a serial terminal. |
- | All the outputs are printed from the UART to the USER USB port using P0.6 and P0.7, and can be read on the PC using a serial terminal program, such as Putty or Tera Term. | + | All the outputs are printed from the UART to the USER USB port using P0.6 and P0.7, and can be read on the PC using a serial terminal program, such as Putty or Tera Term. The user must ensure that the USB cable is connected to the USER USB port in order to read back values in Putty. |
- | ===== Setting up the hardware ===== | + | {{ : |
- | \\ | + | |
- | * To program the base board, set the jumpers as shown in the next figure. The important jumpers are highlighted in red. | + | ===== Demo Requirements ===== |
- | {{: | + | |
- | * Plug the EVAL-ADT7420-PMDZ | + | The following is a list of items needed in order to replicate this demo. |
+ | * Hardware | ||
+ | * EVAL-ADICUP360 | ||
+ | | ||
+ | * Mirco USB to USB cable | ||
+ | * PC or Laptop with a USB port | ||
+ | * Software | ||
+ | * ADuCM360_demo_adt7420_pmdz software | ||
+ | * CrossCore Embedded Studio | ||
+ | * ADuCM36x DFP (1.0.2 or higher) | ||
+ | * CMSIS ARM Pack (4.3.0 or higher) | ||
+ | * Serial Terminal Program | ||
+ | * Such as Putty or Tera Term | ||
- | * Power EVAL-ADICUP360 base board via the Debug USB. | + | ===== Setting up the hardware ===== |
- | \\ | + | - To program the base board, set the jumpers/ |
- | ===== Obtaining | + | - Plug the EVAL-ADT7420-PMDZ PMOD in the EVAL-ADICUP360 base board, via the PMOD_I2C port (P10). |
- | \\ | + | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) |
- | We recommend not opening | + | ===== Obtaining |
- | To learn how to import | + | There are two basic ways to program |
+ | | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github: | + | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. |
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_adt7420** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
+ | Prebuilt ADT7420 Bin File | ||
+ | * [[https:// | ||
+ | Complete ADT7420 Source Files | ||
+ | * [[https:// | ||
- | [[https:// | ||
- | |||
</ | </ | ||
- | \\ | + | <WRAP center round info 80%> |
- | ===== Importing the ADuCM360_demo_adt7420_pmdz project ===== | + | For more information |
- | \\ | + | </ |
- | The necessary instructions | + | |
- | \\ | + | ===== Configuring |
- | ===== Debugging | + | |
- | \\ | + | |
- | * A debug configuration must be set up for this project in order to have the possibility to program and to debug the **ADuCM360_demo_adt7420_pmdz** project. To do this, follow the instructions from [[resources: | + | |
- | * Make sure the target board is connected to the computer (via **DEBUG USB**) and using the tool bar, navigate | + | Configure |
- | + | < | |
- | {{ : | + | |
- | * Use step-by-step execution or directly run the program. | + | /* ADT7420 I2C Address */ |
- | + | #define ADT7420_ADDRESS | |
- | After completion | + | |
- | \\ | + | </code> |
- | ===== Project structure ===== | + | |
- | \\ | + | |
- | The **ADuCM360_demo_adt7420_pmdz** project use basic ARM Cortex-M C/C++ Project structure. | + | |
- | This project contains: system initialization part - disabling watchdog, setting system clock, enabling clock for peripheral; port configuration for I2C, temperature sensor data; I2C read/write functions; threshold monitoring. | + | |
- | \\ | + | |
- | \\ | + | |
- | {{: | + | |
- | In the **src** and **include** folders you will find the source and header files related to adt7420_pmdz application. You can modify those files as appropriate for your application. The // | + | Configure |
- | * **ADT7420 Configuration Register** - // | + | |
< | < | ||
uint8_t ui8configAdt7420 = (FAULT_TRIGGER_4 | CT_PIN_POLARITY | INT_PIN_POLARITY | INT_CT_MODE |CONTINUOUS_CONVERSION_MODE | RESOLUTION_13_BITS); | uint8_t ui8configAdt7420 = (FAULT_TRIGGER_4 | CT_PIN_POLARITY | INT_PIN_POLARITY | INT_CT_MODE |CONTINUOUS_CONVERSION_MODE | RESOLUTION_13_BITS); | ||
- | /** | + | /* False Trigger Count */ |
- | #define FAULT_TRIGGER_1 | + | #define FAULT_TRIGGER_1 |
- | #define FAULT_TRIGGER_2 | + | #define FAULT_TRIGGER_2 |
- | #define FAULT_TRIGGER_3 | + | #define FAULT_TRIGGER_3 |
- | #define FAULT_TRIGGER_4 | + | #define FAULT_TRIGGER_4 |
- | #define CT_PIN_POLARITY | + | /* Alarm Logic Levels */ |
- | #define INT_PIN_POLARITY | + | #define CT_PIN_POLARITY |
- | #define INT_CT_MODE - 1 fault triggers an interrupt | + | #define INT_PIN_POLARITY |
- | #define CONTINUOUS_CONVERSION_MODE - Continuous conversion | + | /* Interrupt Mode */ |
- | #define ONE_SHOT_MODE - One shot conversion () | + | # |
- | #define ONE_SAMPLE_PER_SECOND_MODE - One second conversion | + | |
- | # | + | |
- | #define RESOLUTION_13_BITS | + | /* Conversion Mode */ |
- | #define RESOLUTION_16_BITS | + | #define CONTINUOUS_CONVERSION_MODE |
+ | #define ONE_SHOT_MODE | ||
+ | #define ONE_SAMPLE_PER_SECOND_MODE | ||
+ | #define SHUTDOWN_MODE | ||
+ | |||
+ | /* Resolution */ | ||
+ | #define RESOLUTION_13_BITS | ||
+ | #define RESOLUTION_16_BITS | ||
- | **/ | ||
</ | </ | ||
- | \\ | ||
- | * **ADT7420 I2C Address**- // | ||
- | < | ||
- | #define ADT7420_ADDRESS | + | Assign values to your different temperature setpoints and alarms/ |
- | </ | ||
- | * **High Temperature Interrupt** - // | ||
< | < | ||
- | #define TEMP_HIGH_SETPOINT | + | /* Temperature monitoring parameters */ |
+ | #define TEMP_HIGH_SETPOINT | ||
+ | #define TEMP_LOW_SETPOINT | ||
+ | #define TEMP_CRITICAL_SETPOINT | ||
+ | #define TEMP_HYSTERSIS_SETPOINT | ||
</ | </ | ||
- | * **Low Temperature Interrupt** - // | ||
- | < | ||
- | #define TEMP_LOW_SETPOINT | + | ===== Outputting Data ===== |
- | </ | + | ==== Serial Terminal Output ==== |
- | * **Critical Temperature Interrupt** | + | |
- | < | + | - Once complete you will need to switch |
+ | - Then follow the UART settings below with the serial terminal program. | ||
+ | \\ | ||
- | #define TEMP_CRITICAL_SETPOINT | + | Following is the UART configuration. |
+ | Select COM Port | ||
+ | Baud rate: 9600 | ||
+ | Data: 8 bit | ||
+ | Parity: none | ||
+ | Stop: 1 bit | ||
+ | Flow Control: none | ||
+ | \\ | ||
- | </code> | + | The user must press the **<ENTER>** key each time they want to display the results. |
- | * ** Temperature Hysteresis** | + | {{ : |
- | < | + | |
- | #define TEMP_HYSTERSIS_SETPOINT | + | ===== How to use the Tools ===== |
+ | |||
+ | The official tool we promote for use with the EVAL-ADICUP360 is CrossCore Embedded Studio. | ||
+ | |||
+ | ==== Importing ==== | ||
+ | |||
+ | For more detailed instructions on importing this application/ | ||
+ | |||
+ | ==== Debugging ==== | ||
+ | |||
+ | For more detailed instructions on importing this application/ | ||
+ | |||
+ | ==== Project Structure ==== | ||
- | </ | ||
\\ | \\ | ||
- | The **system** folder contains system related files (try not to change these files): | + | This is the **ADuCM360_demo_adt7420_pmdz** project structure. |
- | * **ADuCM360** – contains low levels drivers for ADuCM360 microcontroller. | + | This project |
- | * **CMSIS** – contains | + | |
- | * **cortexm** – contains files for system management (start-up, reset, exception handler). | + | |
\\ | \\ | ||
+ | \\ | ||
+ | {{: | ||
+ | |||
+ | In the **src** and **include** folders you will find the source and header files related to adt7420_pmdz application. You can modify those files as appropriate for your application. The // | ||
+ | | ||
+ | \\ | ||
+ | The **RTE** folder contains device and system related files: | ||
+ | * **Device Folder** – contains low levels drivers for ADuCM360 microcontroller.(try not to edit these files) | ||
+ | * **system.rteconfig** - Allows the user to select the peripherial components they need, along with the startup and ARM cmsis files needed for the project. | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
+ | // End of Document // |