This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [14 Mar 2021 05:46] – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [14 Mar 2021 06:08] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 44: | Line 44: | ||
- Dragging and Dropping the .Bin to the MBED drive | - Dragging and Dropping the .Bin to the MBED drive | ||
- Building, Compiling, and Debugging using CCES | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. | ||
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. |