This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [20 Oct 2017 19:52] – Brandon Bushey | resources:eval:user-guides:eval-adicup360:reference_designs:demo_adt7420 [14 Mar 2021 06:08] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 39: | Line 39: | ||
- Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM360_demo_adt7420_pmdz** can be found on Github: | + | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. |
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_adt7420** demo can be found here: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
+ | Prebuilt ADT7420 Bin File | ||
+ | * [[https:// | ||
+ | Complete ADT7420 Source Files | ||
+ | * [[https:// | ||
- | [[https:// | ||
- | |||
</ | </ | ||
+ | |||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
- | For more information on importing, debugging, or other tools related questions, please see the [[https:// | + | For more information on importing, debugging, or other tools related questions, please see the [[/ |
</ | </ | ||