This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0396 [28 Oct 2016 10:06] – Added Images and links to sensors JB Chua | resources:eval:user-guides:eval-adicup360:hardware:cn0396 [29 Jul 2021 05:22] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 3: | Line 3: | ||
[[ADI> | [[ADI> | ||
- | The circuit shown in below uses the [[http:// | + | The circuit shown in below uses the [[adi>ADA4528-2|ADA4528-2]], |
- | The [[http:// | + | The [[adi>ADR3412|ADR3412]] precision, low noise, micropower reference establishes the 1.2 V common-mode, |
- | For applications where measuring fractions of ppm gas concentration is important, using the [[http:// | + | For applications where measuring fractions of ppm gas concentration is important, using the [[adi>ADA4528-2|ADA4528-2]] and the [[adi>ADR3412|ADR3412]] makes the circuit performance suitable for interfacing with a 16-bit ADC, such as the [[adi>AD7790|AD7790]]. |
An ADT7310 16-Bit Digital SPI Temperature Sensor is also included in the circuit to allow for monitoring of environmental temp. This allows for correction of the temperature effects on the sensor. | An ADT7310 16-Bit Digital SPI Temperature Sensor is also included in the circuit to allow for monitoring of environmental temp. This allows for correction of the temperature effects on the sensor. | ||
Line 20: | Line 20: | ||
* EVAL-CN0396-ARDZ Circuit Evaluation Board | * EVAL-CN0396-ARDZ Circuit Evaluation Board | ||
* EVAL-ADICUP360 Development Board / Arduino R3 compatible processor Board | * EVAL-ADICUP360 Development Board / Arduino R3 compatible processor Board | ||
- | * Power supply: 6 V or 6 V wall wart | + | * Power supply: 6 V or 6 V wall wart (not needed if plugged into the PC via USB) |
* 4-Electrode Electrochemical Gas Sensor (CO-H2S sensor is provided with the evaluation board) | * 4-Electrode Electrochemical Gas Sensor (CO-H2S sensor is provided with the evaluation board) | ||
* Environmental chamber | * Environmental chamber | ||
Line 50: | Line 50: | ||
Pin Compatible Sensors: | Pin Compatible Sensors: | ||
- | * [[http:// | + | * [[https:// |
- | * [[http:// | + | * [[https:// |
* DD-Scientific GS+4DT | * DD-Scientific GS+4DT | ||
+ | |||
+ | **Sensor Socket Connection** | ||
+ | \\ | ||
+ | {{: | ||
+ | ^ Pin Name ^ Description ^ | ||
+ | | WE1 | Working Electrode (CO gas electrode for COH-A2 sensor) | | ||
+ | | CE | Counter Electrode | | ||
+ | | WE2 | Working Electrode (H2S gas electrode for COH-A2 sensor) | | ||
+ | | RE | Reference Electrode | | ||
<WRAP left round tip 80%> | <WRAP left round tip 80%> | ||
Line 65: | Line 74: | ||
* **AD7798_CS** - selects either Arduino Pin D9 or D10 as CS for AD7798 ADC. | * **AD7798_CS** - selects either Arduino Pin D9 or D10 as CS for AD7798 ADC. | ||
- | ^ JP1 Connections ^ Arduino Pin (P??) ^ | + | ^ AD7798_CS |
- | | Across | + | | Jumper |
- | | Across | + | | Jumper |
* **AD5270_CS** - selects either Arduino Pin D5 or D6 as CS for AD5270 Digital Rheostat | * **AD5270_CS** - selects either Arduino Pin D5 or D6 as CS for AD5270 Digital Rheostat | ||
- | ^ JP2 Connections ^ Arduino Pin (P??) ^ | + | ^ AD5270_CS |
- | | Across | + | | Jumper |
- | | Across | + | | Jumper |
* **ADT7310_CS** - selects either Arduino Pin D3 or D4 as CS for ADT7310 Digital Temp Sensor | * **ADT7310_CS** - selects either Arduino Pin D3 or D4 as CS for ADT7310 Digital Temp Sensor | ||
- | ^ JP3 Connections ^ Arduino Pin (P??) ^ | + | ^ ADT7310_CS |
- | | Across | + | | Jumper |
- | | Across | + | | Jumper |
- | + | ||
- | ---- | + | |
- | + | ||
- | ===== Digital | + | |
- | + | ||
- | Talk about SPI on the Arduino side header and on the ICSP header, and where to find clk, miso,mosi etc. | + | |
---- | ---- | ||
Line 92: | Line 95: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>cn0396-designsupport|EVAL-CN0396-ARDZ Design & Integration Files]] |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 102: | Line 105: | ||
====== Software ====== | ====== Software ====== | ||
- | * [[resources: | + | * [[resources: |
- | * [[https:// | + | * [[resources:eval:user-guides: |
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
- | {{navigation EVAL-ADICUP360# | + | //End of Document// |