This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0395 [07 Jul 2017 17:13] – [Software] Ramon Glenn Amparo | resources:eval:user-guides:eval-adicup360:hardware:cn0395 [29 Jul 2021 05:20] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 2: | Line 2: | ||
- | \\ | ||
The circuit below is an arduino compatible, single supply 16-bit volatile organic compound detector using a metal oxide sensor. It uses [[ADI> | The circuit below is an arduino compatible, single supply 16-bit volatile organic compound detector using a metal oxide sensor. It uses [[ADI> | ||
- | \\ | ||
- | {{ : | + | {{ : |
- | \\ | ||
[[ADI> | [[ADI> | ||
+ | {{ : | ||
=====Connectors and Jumper Configurations===== | =====Connectors and Jumper Configurations===== | ||
+ | {{ : | ||
+ | |||
==== Headers ==== | ==== Headers ==== | ||
- | {{ : | + | === P1 === |
+ | |||
+ | The current output DAC, [[ADI> | ||
+ | |||
+ | For higher output voltages that 2V, tie the ENCOMP pin to +5V to maintain the output stability of the part. | ||
+ | |||
+ | === P2 === | ||
P2 header selects the current path from the current output DAC, [[ADI> | P2 header selects the current path from the current output DAC, [[ADI> | ||
- | | Silkscreen | + | ^ Silkscreen |
| RCAL1 | 71.5Ω | | RCAL1 | 71.5Ω | ||
| RCAL1 | 10.0Ω | | RCAL1 | 10.0Ω | ||
| RH+ | Heating Resistor| 5 & 6| | | RH+ | Heating Resistor| 5 & 6| | ||
- | |||
- | A jumper | ||
==== Sensor ==== | ==== Sensor ==== | ||
Line 34: | Line 38: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
- | + | ||
+ | If you are using a different sensor, you will need to wire in the appropriate signals into the board via the screw terminal (P8). This also means that you will have to remove the TGS8100 sensor that comes on the board by default. | ||
+ | === P8 === | ||
+ | |||
+ | ^ Silkscreen Name ^ Pin Number ^ Description ^ | ||
+ | | RH+ | Pin 1 | Postive Pin of Heating Resistor | | ||
+ | | AGND | Pin 2 | Negative Pin of Heating Resistor| | ||
+ | | RS+ | Pin 3 | Postive Pin of Sensing Resistor| | ||
+ | | AGND | Pin 4 | Negative Pin of Sensing Resistor| | ||
====Spacers==== | ====Spacers==== | ||
Line 43: | Line 56: | ||
Sense resistors (RSN) can be calculated by using the formula below: | Sense resistors (RSN) can be calculated by using the formula below: | ||
- | RSN=4.096/ | + | RSN= 4.096/(10* Full Scale Current) |
====Button==== | ====Button==== | ||
- | Pressing push button S2 resets | + | Pressing push button S2 allows the user to do a hard reset of the temperature and humidity sensor [[https:// |
===== Schematic, PCB Layout, Bill of Materials ===== | ===== Schematic, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>cn0395-designsupport|EVAL-CN0395-ARDZ Design & Integration Files]] |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 60: | Line 72: | ||
===== Software ===== | ===== Software ===== | ||
- | * [[https:// | + | * [[/ |
+ | |||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
- | {{navigation EVAL-ADICUP360# | + | //End of Document// |