This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:hardware:cn0394 [10 Oct 2016 11:53] – Robert Lee | resources:eval:user-guides:eval-adicup360:hardware:cn0394 [03 Jan 2021 21:46] – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== EVAL-CN0394-ARDZ Shield | + | ====== EVAL-CN0394-ARDZ Shield ====== |
- | The [[http:// | + | ===== Overview ===== |
- | //< | + | The [[adi>cn0394|EVAL-CN0394-ARDZ shield]] is a single supply, multi channel thermocouple temperature meter. The CN0394 uses [[adi> |
+ | |||
+ | {{ : | ||
===== Equipment ===== | ===== Equipment ===== | ||
* EVAL-CN0394-ARDZ Circuit Evaluation Board | * EVAL-CN0394-ARDZ Circuit Evaluation Board | ||
- | * [[http:// | + | * [[adi>EVAL-ADICUP360|EVAL-ADICUP360]] Development Board |
- | * B, | + | * Any combination of B, E, J, K, N, R, S, T type thermocouples |
- | * PC with Microsoft Windows 7 64bit or later and USB2.0 port or higher | + | * PC with Microsoft Windows 7 64-bit |
- | * Serial terminal software | + | * Serial terminal software |
+ | * Such as Putty or Tera Term | ||
- | ====== General Setup ====== | + | ===== General Setup ===== |
* Connect the EVAL-CN0394-ARDZ to EVAL-ADICUP360 board | * Connect the EVAL-CN0394-ARDZ to EVAL-ADICUP360 board | ||
Line 19: | Line 22: | ||
* Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | * Connect the EVAL-ADICUP360 **USER** USB port to PC with USB cable | ||
- | ====== Connectors and Jumper | + | ===== Connectors and Configurations ===== |
- | ===== Chip Select | + | ==== Thermocouple Connectors |
+ | |||
+ | Each of the four(4) channels uses an Omega style connector for the thermocouples, | ||
+ | |||
+ | There is an RTD beneath the copper tabs of each connector which is used to measure the cold junction temperature. | ||
+ | |||
+ | ==== Analog Sensor Inputs ==== | ||
+ | |||
+ | The analog outputs of each thermocouple channel and each RTD channel are connected directly to connector P6. Each of these analog voltages is passed directly to the ADuCM360 on the EVAL-ADICUP360 board. | ||
+ | |||
+ | ^ P6 Pin Connections ^ Sensor/ | ||
+ | | Pin 1 | Thermocouple+ (P1) | | ||
+ | | Pin 2 | Thermocouple+ (P2) | | ||
+ | | Pin 3 | Thermocouple+ (P3) | | ||
+ | | Pin 4 | Thermocouple+ (P4) | | ||
+ | | Pin 5 | RTD Output (R1) | | ||
+ | | Pin 6 | RTD Output (R2) | | ||
+ | | Pin 7 | RTD Output (R3) | | ||
+ | | Pin 8 | RTD Output (R4) | | ||
+ | |||
+ | ^ P7 Pin Connections ^ Sensor/ | ||
+ | | Pin 1 | RTD Common | | ||
+ | | Pin 4 | Thermocouple Common (-) | | ||
+ | | Pin 7 | Voltage Reference | | ||
+ | |||
+ | ===== Schematic, PCB Layout, Bill of Materials | ||
- | ====== Schematic, PCB Layout, Bill of Materials ====== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[www.analog.com/ | + | EVAL-CN0394-ARDZ Design & Integration Files |
- | * Schematics | + | * {{: |
- | * PCB Layout | + | * {{: |
- | * Bill of Materials | + | * {{: |
- | * Allegro Project | + | * {{: |
</ | </ | ||
- | ====== Software | + | ===== Software ===== |
- | * [[resources: | + | * [[resources: |
- | * AduCM360 | + | * ADuCM360 |
* [[https:// | * [[https:// | ||
- | |||
{{navigation EVAL-ADICUP360# | {{navigation EVAL-ADICUP360# | ||
+ |