Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:user-guides:eval-adicup360:hardware:cn0326 [19 May 2017 03:13] – [Sensor Probe Requirements] erbe reyta | resources:eval:user-guides:eval-adicup360:hardware:cn0326 [24 May 2017 19:30] – Brandon Bushey |
---|
==== Sensor Probe Requirements ==== | ==== Sensor Probe Requirements ==== |
| |
When using the CN0326 PMOD board, a general purpose pH probe with BNC connecter can be used for pH measurement. An example of a pH probe that can be used is a product from [[https://www.atlas-scientific.com/product_pages/probes/ph_probe.html|Atlas]] or from [[https://www.hach.com/radiometer-probes/radiometer-analytical-probes/family?productCategoryId=35547627768|Hach]]. For temperature compensation, an RTD sensor with RCA connector can be used. An example is from [[https://www.atlas-scientific.com/product_pages/probes/pt1000.html|Atlas]] or from [[http://sea.omega.com/ph/subsection/rtd-elements-with-lead-wires-attached.html|Omega]]. These sensors are required in order to run and capture analog signal from a sample solution and the connections can be seen on the diagram as shown below. | When using the CN0326 PMOD board, a general purpose pH probe with BNC connector can be used for pH measurement. An example of a pH probe that can be used is a product from [[https://www.atlas-scientific.com/product_pages/probes/ph_probe.html|Atlas]] or from [[https://www.hach.com/radiometer-probes/radiometer-analytical-probes/family?productCategoryId=35547627768|Hach]]. For temperature compensation, an RTD sensor with RCA connector can be used. An example is from [[https://www.atlas-scientific.com/product_pages/probes/pt1000.html|Atlas]] or from [[http://sea.omega.com/ph/subsection/rtd-elements-with-lead-wires-attached.html|Omega]]. These sensors are required in order to run and capture analog signal from a sample solution and the connections can be seen on the diagram as shown below. |
| |
{{ :resources:eval:user-guides:eval-adicup360:hardware:cn0326:sensor_interface.jpg |}} | {{ :resources:eval:user-guides:eval-adicup360:hardware:cn0326:sensor_interface.jpg |}} |
===== Software examples ===== | ===== Software examples ===== |
| |
* [[resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0326|CN0326 Demo]] | * [[resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0326|ADICUP360 + CN0326 Demo]] |
| |
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== |