This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [03 Mar 2018 09:39] – [CrossCore Embedded Studio Quickstart User Guide] Andrew McLachlan | resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [08 Nov 2021 17:41] (current) – removed deprecated packs Brandon Bushey | ||
---|---|---|---|
Line 10: | Line 10: | ||
- How to install or upgrade the Analog Devices Packs for CCES | - How to install or upgrade the Analog Devices Packs for CCES | ||
- ADuCM302x Device Family Pack (DFP) | - ADuCM302x Device Family Pack (DFP) | ||
- | - ADICUP3029 Board Support Package (BSP) | ||
- | - Sensor Software Pack | ||
- | - Wi-Fi Software Pack | ||
- | - Bluetooth Software Pack | ||
- How to create a new project for the ADuCM3029 | - How to create a new project for the ADuCM3029 | ||
- How to add startup code and core components to a new project for the ADuCM3029 | - How to add startup code and core components to a new project for the ADuCM3029 | ||
Line 42: | Line 38: | ||
* ADuCM302x Device Family Pack (DFP) | * ADuCM302x Device Family Pack (DFP) | ||
- | * ADICUP3029 Board Support Pack (BSP) | ||
- | * ADI Sensor Software Pack | ||
- | * ADI Wi-Fi Software Pack | ||
- | * ADI BLE Software Pack | ||
* ARM CMSIS Pack | * ARM CMSIS Pack | ||
\\ | \\ | ||
Line 69: | Line 61: | ||
{{ : | {{ : | ||
- | |||
- | ==== ADICUP3029 Board Support Pack (BSP) ==== | ||
- | |||
- | The ADICUP3029 Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the ADICUP3029 Evaluation Board and examples for peripherals on the ADUCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP) 2.0.0. | ||
- | |||
- | For more information on the ADICUP3029 BSP, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\EVAL-ADICUP3029_BSP\1.0.0\Documents\EVAL-ADICUP3029_Users_Guide.pdf) | ||
- | |||
- | ==== ADI Sensor Software Pack ==== | ||
- | |||
- | The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with ADICUP3029 board and associated sensor shields. ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and ADICUP3029 Board Support Package 1.1.0. | ||
- | |||
- | For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf) | ||
- | |||
- | ==== ADI WiFi Software Pack ==== | ||
- | |||
- | Wi-Fi software pack contains source code written to interface the ADuCM3029 with the ESP8266 Wi-Fi radio module. This software package acts as a library that can be used with any platform containing the ADuCM3029 and the ESP8266. | ||
- | |||
- | ADI WiFi Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and ADICUP3029 Board Support Package 1.1.0. | ||
- | |||
- | For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-WifiSoftware\1.0.0\Documents\Wifi_Software_Users_Guide.pdf) | ||
- | |||
- | ==== ADI Bluetooth Software Pack ==== | ||
- | |||
- | BLE software pack contains source code written to interface the ADuCM3029 with the EM9304 radio. This software package acts as a library that can be used with any platform containing the ADuCM3029 and the EM9304. | ||
- | |||
- | The Software pack also includes the currently version of the IoTNode Android application for Bluetooth Low-Energy host connectivity. | ||
- | |||
- | ADI BLE Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and ADICUP3029 Board Support Package 1.1.0. | ||
- | |||
- | For more information on the ADI Bluetooth Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-BleSoftware\1.0.0\Documents\BLE_Software_Users_Guide.pdf) | ||
==== ARM CMSIS Pack ==== | ==== ARM CMSIS Pack ==== |