This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [01 Jun 2017 15:29] – [ADuCM302x Board Support Packs (BSP)] Andrew McLachlan | resources:eval:user-guides:eval-adicup3029:tools:cces_user_guide [08 Nov 2021 17:41] (current) – removed deprecated packs Brandon Bushey | ||
---|---|---|---|
Line 8: | Line 8: | ||
This page covers: | This page covers: | ||
- | - How to install or upgrade the ADuCM302x Device Family Pack (DFP) for CCES | + | - How to install or upgrade the Analog Devices Packs for CCES |
+ | - ADuCM302x Device Family Pack (DFP) | ||
- How to create a new project for the ADuCM3029 | - How to create a new project for the ADuCM3029 | ||
- How to add startup code and core components to a new project for the ADuCM3029 | - How to add startup code and core components to a new project for the ADuCM3029 | ||
Line 18: | Line 19: | ||
- How to create an Intel Hex (.hex) file from an ADuCM3029 application | - How to create an Intel Hex (.hex) file from an ADuCM3029 application | ||
- | ====== Workspace and Projects | + | <WRAP center round info 60%> |
+ | We have a playlist of **YOUTUBE VIDEOS** that can help you understand different functions and features of CrossCore Embedded Studio. [[https:// | ||
+ | </ | ||
+ | |||
+ | ===== Workspace and Projects ===== | ||
A CCES workspace is a folder (e.g. c: | A CCES workspace is a folder (e.g. c: | ||
Line 26: | Line 31: | ||
Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES. | Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES. | ||
- | {{ : | + | {{ : |
+ | |||
+ | ===== How to install or upgrade Packs for CCES ===== | ||
+ | |||
+ | CCES 2.6.0 does not comes with the Analog Device specific packs or the ARM CMSIS Pack file pre-installed. | ||
- | ===== How to install or upgrade the ADuCM302x Device Family Pack (DFP) for CCES ===== | + | * ADuCM302x Device Family Pack (DFP) |
+ | * ARM CMSIS Pack | ||
+ | \\ | ||
+ | {{analogTV> | ||
+ | \\ | ||
- | CCES 2.6.0 does not comes with the ADuCM302x Device Family Pack (DFP) and ARM CMSIS Pack file pre-installed. | + | ==== ADuCM302x Device Family Pack (DFP) ==== |
* To install the ADuCM302x DFP: | * To install the ADuCM302x DFP: | ||
Line 49: | Line 62: | ||
{{ : | {{ : | ||
- | | + | ==== ARM CMSIS Pack ==== |
+ | |||
+ | | ||
* Switch to the CMSIS Pack Manager perspective by selecting //Window | Perspective | Open Perspective | Other... | CMSIS Pack Manager//. | * Switch to the CMSIS Pack Manager perspective by selecting //Window | Perspective | Open Perspective | Other... | CMSIS Pack Manager//. | ||
* Once opened, select //Check for Updates on Web ( blue arrows on the toolbar )//, if you have not already done so. | * Once opened, select //Check for Updates on Web ( blue arrows on the toolbar )//, if you have not already done so. | ||
Line 57: | Line 72: | ||
{{ : | {{ : | ||
- | |||
- | ==== ADuCM302x Board Support Packs (BSP) ==== | ||
- | |||
- | There are two Board Support Packs (BSP) available: one for the ADuCM302x EZ-Kit and one for the ADICUP3029. These BSPs can be installed in the same way as the Device Family Pack (DFP) via the CMSIS Pack Manager perspective. | ||
- | |||
- | === ADuCM302x EZ-Kit Board Support Pack === | ||
- | |||
- | The ADuCM302x EZ-Kit Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the ADuCM302x EZ-Kit and examples for all the peripherals in the ADuCM302x processor. The examples in the BSP depend on the drivers from ADuCM302x Device Family Pack (DFP). The BSP is designed to work with CrossCore Embedded Studio and Keil uVision. | ||
- | |||
- | For more information on the ADuCM302x EZ-Kit BSP, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADuCM302x_EZ_KIT_BSP\2.0.0\Documents\ADuCM302x_EZ-KIT_BSP_Users_Guide.pdf) | ||
- | |||
- | === ADICUP3029 Board Support Pack === | ||
- | |||
- | The ADICUP3029 Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the ADICUP3029 Evaluation Board and examples for peripherals on the ADUCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP). | ||
- | |||
- | For more information on the ADICUP3029 BSP, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\EVAL-ADICUP3029_BSP\1.0.0\Documents\EVAL-ADICUP3029_Users_Guide.pdf) | ||
- | |||
- | ==== ADI Sensor Software Pack ==== | ||
- | |||
- | The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with ADICUP3029 board and associated sensor shields. ADI Sensor Software requires CrossCore Embedded Studio (CCES), ADuCM302x Device Family Pack (DFP) and ADICUP3029 Board Support Pack (BSP). | ||
- | |||
- | For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf) | ||
===== How to create a new project for the ADuCM3029 ===== | ===== How to create a new project for the ADuCM3029 ===== | ||
A project for ADuCM3029 can be created using the New CrossCore Project Wizard. This wizard will guide you through the steps to create a new project. | A project for ADuCM3029 can be created using the New CrossCore Project Wizard. This wizard will guide you through the steps to create a new project. | ||
+ | |||
+ | {{analogTV> | ||
{{ : | {{ : | ||
Line 95: | Line 90: | ||
{{ : | {{ : | ||
- | ===== How to add startup code and core components to a new project for the ADuCM3029 | + | ==== How to add startup code and core components to a new project for the ADuCM3029 ==== |
An out-of-the-box ADuCM3029 project does not have startup code or a linker description file that maps code and data. It is necessary to add these components using the Run-time Environment (RTE) Configuration Editor. | An out-of-the-box ADuCM3029 project does not have startup code or a linker description file that maps code and data. It is necessary to add these components using the Run-time Environment (RTE) Configuration Editor. | ||
Line 115: | Line 110: | ||
- Examples that you have saved to a local drive on your PC. | - Examples that you have saved to a local drive on your PC. | ||
- | - Examples that come with the ADuCM3029 Device Family | + | - Examples that come with the Analog Devices |
- Examples which are in the ADICUP3029 GIT repository (most up to date content). | - Examples which are in the ADICUP3029 GIT repository (most up to date content). | ||
Line 128: | Line 123: | ||
{{ : | {{ : | ||
- | ==== How to Import Examples that come with the ADuCM3029 Device Family Pack (DFP) ==== | + | ==== How to Import Examples that come with the ADuCM3029 Device Family Pack (DFP) or Board Support Packs (BSP) ==== |
- | Examples | + | === Opening CCES Examples |
- Open CMSIS Pack Manager perspective by clicking "Open Perspective" | - Open CMSIS Pack Manager perspective by clicking "Open Perspective" | ||
Line 137: | Line 132: | ||
- A dialog will pop-up showing the location where the example will be copied to. Click //Copy// to copy and open the example project. | - A dialog will pop-up showing the location where the example will be copied to. Click //Copy// to copy and open the example project. | ||
- | {{ : | + | {{ : |
- | The CCES Examples | + | === Opening Examples using the CCES Example |
+ | - Launch the CCES Example Broswer by clicking on //Help --> Browse Examples// | ||
- Select ADuCM302x_DFP[x.y.z] in Product drop-down list, select the example and click Open example. Then the example will be copied to your workspace. | - Select ADuCM302x_DFP[x.y.z] in Product drop-down list, select the example and click Open example. Then the example will be copied to your workspace. | ||
- | + | \\ | |
- | {{ : | + | {{analogTV> |
+ | \\ | ||
==== How to Import Existing Projects from the GIT Repository ==== | ==== How to Import Existing Projects from the GIT Repository ==== | ||
Line 157: | Line 154: | ||
- Click //Next// and then //Finish// | - Click //Next// and then //Finish// | ||
- | {{ : | + | \\ |
- | + | {{analogTV> | |
- | ===== How to build projects for programming the ADuCM3029 ===== | + | \\ |
- | + | ||
- | - Open the C perspective by clicking "Open Perspective" | + | |
- | - Right click on the project and select the //Build Project// | + | |
- | * Or click the //Hammer// icon from the toolbar. | + | |
- | + | ||
- | {{ : | + | |
===== How to configure the Tools Settings used by an ADuCM3029 project ===== | ===== How to configure the Tools Settings used by an ADuCM3029 project ===== | ||
Line 175: | Line 166: | ||
{{ : | {{ : | ||
+ | |||
+ | ==== Enabling/ | ||
+ | |||
+ | \\ | ||
+ | {{analogTV> | ||
+ | \\ | ||
+ | |||
+ | - To enable/ | ||
+ | - Change the // | ||
+ | * Enable semi-hosting by selecting the **rdimon.specs** option. | ||
+ | * Use this option if using the debugger for things like printf() or other similar tools. | ||
+ | * Disable semi-hosting by selecting the **nosys.specs** or **None** options. | ||
+ | * Use this option for standalone embedded operation. | ||
+ | - After configuring your project, click Apply and/or OK. | ||
+ | - Right click on the project and select the //Build Project//. | ||
+ | * Or click the //Hammer// icon from the toolbar. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ===== How to build projects for programming the ADuCM3029 ===== | ||
+ | |||
+ | - Open the C perspective by clicking "Open Perspective" | ||
+ | - Right click on the project and select the //Build Project//. | ||
+ | * Or click the //Hammer// icon from the toolbar. | ||
+ | |||
+ | {{ : | ||
===== How to configure the debug session for an ADuCM3029 application ===== | ===== How to configure the debug session for an ADuCM3029 application ===== | ||
+ | |||
+ | \\ | ||
+ | {{analogTV> | ||
+ | \\ | ||
You will need to create a launch configuration to debug your ADuCM3029 program. | You will need to create a launch configuration to debug your ADuCM3029 program. | ||
Line 192: | Line 213: | ||
{{ : | {{ : | ||
- | ======= Hardware breakpoints are limited in your ADuCM3029 application | + | ==== Hardware breakpoints are limited in your ADuCM3029 application ==== |
- When you click Debug or Apply, you will be prompted with a dialog informing your the Hardware Breakpoints are limited. Click //Yes//. You can opt to not show this dialog again. | - When you click Debug or Apply, you will be prompted with a dialog informing your the Hardware Breakpoints are limited. Click //Yes//. You can opt to not show this dialog again. | ||
Line 202: | Line 223: | ||
- Ensure that you have connected your EVAL-ADICUP3029 board to your computer via the **USB** port (the micro USB connected closest to the DC barrel jack). | - Ensure that you have connected your EVAL-ADICUP3029 board to your computer via the **USB** port (the micro USB connected closest to the DC barrel jack). | ||
- If you are already in the Debug Configurations dialog, then click //Debug//. | - If you are already in the Debug Configurations dialog, then click //Debug//. | ||
- | - If you are in the C Perspective, | + | - If you are in the C Perspective, |
- | + | - You will be prompted to switch perspective to the Debug perspective. Click //Yes//. You can opt to not show this dialog again.{{ : | |
- | {{ : | + | - If your binary (program) was built with semi-hosting enabled, then CCES will warn you that you need to re-build the program when you want to run the program without a debugger attached.{{ : |
- | + | - To change | |
- | - You will be prompted to switch perspective to the Debug perspective. Click //Yes//. You can opt to not show this dialog again. | + | - If this is the first time you have launched OpenOCD, the Windows Firewall may pop-up a window asking for access. |
- | + | ||
- | {{ : | + | |
- | + | ||
- | - If your binary (program) was built with semi-hosting enabled, then CCES will warn you that you need to re-build the program when you want to run the program without a debugger attached. | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | - To disable semi-hosting in your program, visit your project Tools Settings. | + | |
- | - Change | + | |
- | - After configuring your project, click Apply and/or OK. | + | |
- | - Right click on the project and select the //Build Project// | + | |
- | * Or click the //Hammer// icon from the toolbar. | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | - If this is the first time you have launched OpenOCD, the Windows Firewall may pop-up a window asking for access. | + | |
- | + | ||
- | {{ : | + | |
- If everything goes fine, in the Console window, you will see a report without errors. | - If everything goes fine, in the Console window, you will see a report without errors. | ||
* As a reference, the full text should be similar to:< | * As a reference, the full text should be similar to:< | ||
Line 248: | Line 250: | ||
Info : accepting ' | Info : accepting ' | ||
</ | </ | ||
- | - Your program' | + | - Your program' |
+ | - To terminate a debug session, click on the red //Stop// button on the toolbar.{{ : | ||
- | {{ : | + | ===== How to create an Intel Hex (.hex) file or Binary (.bin) file for an ADuCM3029 application ===== |
- | + | ||
- | - To terminate a debug session, click on the red //Stop// button on the toolbar. | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | ===== How to create an Intel Hex (.hex) file from an ADuCM3029 application ===== | + | |
- Ensure that your program is built with semi-hosting disabled by visiting //Tools Settings | Linker | Libraries// and change // | - Ensure that your program is built with semi-hosting disabled by visiting //Tools Settings | Linker | Libraries// and change // | ||
- | - Rebuild your application. | + | - Rebuild your application.{{: |
- | + | - Convert your application into Intel Hex (.hex) or Binary (.bin) format by visiting Tools Settings once more. | |
- | {{ : | + | |
- | + | ||
- | - Convert your application into Intel Hex (.hex) format by visiting Tools Settings once more. | + | |
- Select the Build Steps tab. | - Select the Build Steps tab. | ||
- | - Add the following | + | - Add one of the following |
+ | * Intel Hex (.hex) file command:< | ||
+ | * Binary (.bin) file command:< | ||
- Rebuild your application. | - Rebuild your application. | ||
- | {{ : | + | {{: |
//End of Document// | //End of Document// |