This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_plc_modbus [28 Jan 2021 17:25] – Fixed bad link for digikey Ioana Chelaru | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_plc_modbus [08 Mar 2021 06:12] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 71: | Line 71: | ||
The CP2103 device must be programmed as follows to control the DE signal on the CN0416. Configure Silicon Labs Xpress Configurator as follows to program the device: | The CP2103 device must be programmed as follows to control the DE signal on the CN0416. Configure Silicon Labs Xpress Configurator as follows to program the device: | ||
| IO2 configuration | | IO2 configuration | ||
- | Once the CP2103 is programmed, unplug from the host computer and connect P1 on the ADALM-UARTJTAG to P11 on the CN0416 with a 2x5-socket, 100mil cable such as [[https:// | + | Once the CP2103 is programmed, unplug from the host computer and connect P1 on the ADALM-UARTJTAG to P11 on the CN0416 with a 2x5-socket, 100mil cable such as [[digikey>A3AAH-1006G|AMP A3AAH-1006G]]. Be sure to connect with proper polarity - pin 1 on the ADALM-UARTJTAG must correspond to pin 1 on the CN0416. |
^ CN0416 Setup ^^^^^ | ^ CN0416 Setup ^^^^^ | ||
^ ^ Isolated Full Duplex | ^ ^ Isolated Full Duplex | ||
Line 305: | Line 305: | ||
\\ | \\ | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM3029_demo_cn0435** can be found here: | + | Using the drag and drop method, |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | [[https:// | + | The software for the **ADuCM3029_demo_cn0435** can be found here: |
+ | |||
+ | <WRAP round 80% download> | ||
+ | Prebuilt CN0435 Hex File | ||
+ | * [[https:// | ||
+ | Complete CN0435 Source Files | ||
+ | * [[https:// | ||
</ | </ |