This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [23 Jul 2020 16:35] – [Obtaining the Source Code] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [18 Apr 2022 21:20] (current) – [Available commands] updated screenshot Brandon Bushey | ||
---|---|---|---|
Line 27: | Line 27: | ||
* PC or Laptop with a USB port | * PC or Laptop with a USB port | ||
* Software | * Software | ||
- | * {{ : | + | * {{ : |
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
Line 34: | Line 34: | ||
- Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | ||
- | ===== Configuring | + | ===== Programming |
- | The ADuCM3029_demo_cn0503 does not need any software | + | This application |
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | </ | ||
===== Outputting Data ===== | ===== Outputting Data ===== | ||
Line 66: | Line 74: | ||
| | // | | | // | ||
- | {{ : | + | {{ : |
- | ===== Obtaining the Source Code ===== | ||
- | This application software is used with the ADICUP3029 to demonstrate the capabilities of the CN0537 evaluation board. To upload the CN0537 software to the ADICUP3029, connect both boards together through the Arduino form factor connectors (P1 to P4 on the CN0537) and plug them to a computer through USB. Upon connection, the hardware should appear as a DAPLINK drive on the computer. Drag and drop the CN0537 hex file to the DAPLINK drive to program the ADICUP3029. | ||
- | {{ : | + | ===== UL-217 Testing Results ===== |
- | <WRAP round 80% download> | + | Using both the EVAL-CN0537-ARDZ and the EVAL-CN0537-ALGO, |
- | {{ : | + | <WRAP center round download 60%> |
- | + | {{ : | |
</ | </ | ||
// End of Document // | // End of Document // |