This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [07 Jul 2020 12:02] – [Configuring the Software] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [18 Apr 2022 21:20] (current) – [Available commands] updated screenshot Brandon Bushey | ||
---|---|---|---|
Line 26: | Line 26: | ||
* Mirco USB to USB cable | * Mirco USB to USB cable | ||
* PC or Laptop with a USB port | * PC or Laptop with a USB port | ||
- | * Software | + | * Software |
- | * [[https://github.com/ | + | * {{ :resources: |
- | * CrossCore Embedded Studio (2.8.0 or higher) | + | |
- | * ADuCM302x DFP (3.2.0 or higher) | + | |
- | * ADICUP3029 BSP (1.1.0 or higher) | + | |
- | * Serial Terminal Program | + | |
- | * Such as Putty or Tera Term | + | |
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== | ||
Line 39: | Line 34: | ||
- Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | ||
- | ===== Configuring | + | ===== Programming |
- | The ADuCM3029_demo_cn0503 does not need any software | + | This application |
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | </ | ||
===== Outputting Data ===== | ===== Outputting Data ===== | ||
Line 52: | Line 55: | ||
^ Function ^ Command ^ Description ^ Example ^ | ^ Function ^ Command ^ Description ^ Example ^ | ||
- | ^ General | + | ^ Application |
| | //h// | Display available commands. | | | | | //h// | Display available commands. | | | ||
- | | | //stts// | + | | | //s// | Put the device in GO mode and stream data from the device to the terminal.\\ <//no//> = number of samples |
- | ^ Internal register commands ^ | | | | + | | | //i// | Stop the stream.\\ <//opt//> = 1 to put the program in idle mode, 0 to keep the program in streaming mode, but stop streaming. | | |
- | | | //r// | Display voltage or current on the selected channel.\\ <//chan//> = channel | + | | | //ms// |
- | | | // | + | | | //os// |
- | ^ HART commands ^ | | + | | | //og// |
- | | | //he// | + | | | //ra// |
- | | | //hd// | Disable HART channel. | | | + | | | //n// | Insert a note into the stream and also the SD card log if started. | n Note 1 = print 'Note 1' on th terminal stream and SD card log if started. | |
- | | | //hcc// | Select wanted channel.\\ <//chan//> = Channel | + | | | //ar// |
- | | | //ht// | + | | | //hc// |
- | | | //hg// | + | ^ SD card commands ^ ^ ^ ^ |
- | | | //hcz// | Send command zero with the specified number of FFs in the preambule.\\ <// | + | | | //fo// |
- | | | //hpt// | Send command zero with the specified number of FFs in the preambule.\\ <// | + | | | //fc// |
- | ^ ADC commands | | | + | ^ Device commands ^ ^ ^ ^ |
- | | | //arr// | Display value of ADC register | + | | | //rr// |
- | | | //awr// | Change value of the ADC register of the given address.\\ <//reg//> = address of the register.\\ <// | + | | | //rw// |
- | | | //ags// | Get a specific number of samples from the given channel.\\ <// | + | | | //rd// |
- | | | // | + | |
- | | | //asf// | Set filter option.\\ <// | + | |
- | | | // | + | |
- | | | //adp// | Select postfilter.\\ <//opt//> = selected postfilter option. | | | + | |
- | | | //asp// | Reset controller, parameters and faults | | | + | |
- | | | + | |
- | | | //aowd// | Disable open wire detection. | | | + | |
- | ^ EEPROM commands ^ | | | + | |
- | | | //de// | + | |
- | {{ : | + | {{ : |
- | ===== Obtaining the Source Code ===== | ||
- | We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace. | ||
- | The source code and include files of the **ADuCM3029_demo_cn0414** can be found here: | + | ===== UL-217 Testing Results ===== |
- | <WRAP round 80% download> | + | Using both the EVAL-CN0537-ARDZ and the EVAL-CN0537-ALGO, |
- | [[https:// | + | <WRAP center round download 60%> |
- | + | {{ :resources: | |
- | [[| AduCM3029_demo_cn0414.HEX]] | + | |
- | + | ||
</ | </ | ||
- | |||
- | ===== How to use the Tools ===== | ||
- | |||
- | The official tool we promote for use with the EVAL-ADICUP3029 is CrossCore Embedded Studio. | ||
- | |||
- | ==== Importing ==== | ||
- | |||
- | For more detailed instructions on importing this application/ | ||
- | |||
- | ==== Debugging ==== | ||
- | |||
- | For more detailed instructions on importing this application/ | ||
- | |||
- | ==== Project Structure ==== | ||
- | |||
- | The program is composed of two main parts: | ||
- | - Board setup with initial values. | ||
- | - Main process. | ||
- | |||
- | {{ : | ||
- | |||
- | Board setup initializes **UART**, **SPI** and **I2C** communication and verifies if there is an active **EVAL-CN0414-ARDZ** board connected by reading the AD4111 ID register. Here is also initialized the update timer for the internal channel registers. | ||
- | |||
- | {{ : | ||
- | |||
- | The main process routine implements the **CLI** and calls the commands input by the user. This routine also checks the flags asserted in the asynchronous events (the update channel register flag, the HART received flag and the floating channel flags) and calls the appropriate handler methods. There is also a flag asserted by the channel register update rate and the **ADC** output data rate. If the update rate would be too close to the output data rate, the actual update rate might slow down to be possible for the program to maintain all functionality. The update rate may never be bigger or equal to the **ADC** output data rate divided by 8 (for 8 channels). | ||
- | |||
- | {{ : | ||
- | |||
- | The flow chart below represents the way the channel registers are updated. Only one channel is active at any one time (the channel that must be read). | ||
- | |||
- | {{ : | ||
// End of Document // | // End of Document // |