This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [31 Jul 2020 18:14] – added test result doc from Intertek Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [22 Mar 2021 15:12] – Adding some clarity Brandon Bushey | ||
---|---|---|---|
Line 34: | Line 34: | ||
- Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ : | ||
- | ===== Configuring | + | ===== Programming |
- | The ADuCM3029_demo_cn0503 does not need any software | + | This application |
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP round 80% download> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | </ | ||
===== Outputting Data ===== | ===== Outputting Data ===== | ||
Line 67: | Line 75: | ||
{{ : | {{ : | ||
- | |||
- | ===== Obtaining the Source Code ===== | ||
- | |||
- | This application software is used with the ADICUP3029 to demonstrate the capabilities of the CN0537 evaluation board. To upload the CN0537 software to the ADICUP3029, connect both boards together through the Arduino form factor connectors (P1 to P4 on the CN0537) and plug them to a computer through USB. Upon connection, the hardware should appear as a DAPLINK drive on the computer. Drag and drop the CN0537 hex file to the DAPLINK drive to program the ADICUP3029. | ||
- | |||
- | {{ : | ||
- | |||
- | <WRAP round 80% download> | ||
- | |||
- | {{ : | ||
- | |||
- | </ | ||
===== UL-217 Testing Results ===== | ===== UL-217 Testing Results ===== | ||
Line 87: | Line 83: | ||
{{ : | {{ : | ||
</ | </ | ||
- | |||
// End of Document // | // End of Document // |