Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [24 Jul 2020 02:12] – [Demo Requirements] Travis Collinsresources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0537 [18 Apr 2022 21:20] (current) – [Available commands] updated screenshot Brandon Bushey
Line 34: Line 34:
   - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0537_system_pc.jpg |}}   - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0537_system_pc.jpg |}}
  
-===== Configuring the Software =====+===== Programming the Firmware =====
  
-The ADuCM3029_demo_cn0503 does not need any software configurationIt can be built and run as is+This application software is used with the ADICUP3029 to demonstrate the capabilities of the CN0537 evaluation boardTo upload the CN0537 software to the ADICUP3029, connect both boards together through the Arduino form factor connectors (P1 to P4 on the CN0537) and plug them to a computer through USB. Upon connection, the hardware should appear as a DAPLINK drive on the computer. Drag and drop the ADuCM3029_demo_cn0537.hex file to the DAPLINK drive to program the ADICUP3029. 
 + 
 +{{ :resources:eval:user-guides:circuits-from-the-lab:cn0537:cn0537_uploading_hex_file.png?nolink&600 |}} 
 + 
 +<WRAP round 80% download> 
 + 
 +{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:aducm3029_demo_cn0537_hex.zip | Smoke detector demo software .hex file}} 
 +  
 +</WRAP>
  
 ===== Outputting Data ===== ===== Outputting Data =====
Line 66: Line 74:
 |  | //rd//                 | Read and display all device registers in one command. |  | |  | //rd//                 | Read and display all device registers in one command. |  |
  
-{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0537_cli.png |}}+{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0537_putty_update.png |}}
  
-===== Obtaining the Source Code ===== 
  
-This application software is used with the ADICUP3029 to demonstrate the capabilities of the CN0537 evaluation board. To upload the CN0537 software to the ADICUP3029, connect both boards together through the Arduino form factor connectors (P1 to P4 on the CN0537) and plug them to a computer through USB. Upon connection, the hardware should appear as a DAPLINK drive on the computer. Drag and drop the CN0537 hex file to the DAPLINK drive to program the ADICUP3029. 
  
-{{ :resources:eval:user-guides:circuits-from-the-lab:cn0537:cn0537_uploading_hex_file.png?nolink&600 |}}+===== UL-217 Testing Results =====
  
-<WRAP round 80% download>+Using both the EVAL-CN0537-ARDZ and the EVAL-CN0537-ALGO, the setup was tested at a certified testing facility (Intertek) and passed all the smoke sensor aspects of the UL-217 8th Ed. standards.  You can view the entire report here.
  
-{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0357:aducm3029_demo_cn0537_hex.zip Smoke detector demo software .hex file}} +<WRAP center round download 60%> 
- +{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:cn0357:intertek_test_report_on_eval-cn0537-algo.pdf |UL-217 8th Edtesting and results document}}
 </WRAP> </WRAP>
  
 // End of Document // // End of Document //
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_cn0537.txt · Last modified: 18 Apr 2022 21:20 by Brandon Bushey