This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0414 [16 Nov 2018 14:08] – [Obtaining the Source Code] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_cn0414 [12 Feb 2019 14:38] – Correct application name Andrei Drimbarean | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== PLC Arduino Shield Input Demo ====== | ====== PLC Arduino Shield Input Demo ====== | ||
- | The **ADuCM_demo_cn0414** project provides a solution to control a **PLC** or **DCS** input system using the **EVAL-CN0414-ARDZ** and the **EVAL-ADICUP3029**. It uses an **ADC** with 4 differential voltage channels and 4 current channels and boasts low power **Open-Wire Detection** capabilities and **HART** communication. It has a 32kb EEPROM memory that can also be used to identify the board and is controlled via a command line interface (**CLI**). | + | The **ADuCM3029_demo_cn0414** project provides a solution to control a **PLC** or **DCS** input system using the **EVAL-CN0414-ARDZ** and the **EVAL-ADICUP3029**. It uses an **ADC** with 4 differential voltage channels and 4 current channels and boasts low power **Open-Wire Detection** capabilities and **HART** communication. It has a 32kb EEPROM memory that can also be used to identify the board and is controlled via a command line interface (**CLI**). |
===== General Description/ | ===== General Description/ | ||
Line 7: | Line 7: | ||
The **ADuCM_demo_cn0414** project uses **EVAL-CN0414-ARDZ** to provide a complete, fully isolated and highly flexible, four channel analog input system. The **EVAL-CN0414-ARDZ** is suitable for programmable logic controllers (**PLC**) and distributed control system (**DCS**) applications that require multiple voltage inputs. It boasts **open wire detection** and has **HART**-compatible, | The **ADuCM_demo_cn0414** project uses **EVAL-CN0414-ARDZ** to provide a complete, fully isolated and highly flexible, four channel analog input system. The **EVAL-CN0414-ARDZ** is suitable for programmable logic controllers (**PLC**) and distributed control system (**DCS**) applications that require multiple voltage inputs. It boasts **open wire detection** and has **HART**-compatible, | ||
- | The circuit can be divided into the following parts: the ADC, the input channels, the HART modem and the memory. | + | The circuit can be divided into the following parts: the ADC, the input channels, the HART modem and the memory. |
- | FIXME! MAYBE LINK TO APP NOTE | + | |
The **ADC** is the core of the **EVAL-CN0414-ARDZ** shield. It is an [[adi> | The **ADC** is the core of the **EVAL-CN0414-ARDZ** shield. It is an [[adi> |