This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxl372 [01 Feb 2018 10:30] – [Setting up the Hardware] Mircea Caprioru | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adxl372 [08 Mar 2021 09:04] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 39: | Line 39: | ||
* P11 -> Pin 1-2 | * P11 -> Pin 1-2 | ||
* P12 -> Pin 1-2 | * P12 -> Pin 1-2 | ||
- | {{ : | + | {{ : |
- Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | ||
Line 82: | Line 82: | ||
\\ | \\ | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM3029_Asset_Health_demo** can be found here: | + | Using the drag and drop method, |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | FIXME! | + | The software for the **ADuCM3029_Asset_Health** can be found here: |
- | [[https:// | + | <WRAP round 80% download> |
+ | Prebuilt ADXL372 Hex File | ||
+ | * [[https:// | ||
+ | Complete ADXL372 Source Files | ||
+ | * [[https:// | ||
</ | </ | ||
- | |||
===== How to use the Tools ===== | ===== How to use the Tools ===== | ||
Line 110: | Line 115: | ||
==== Project Structure ==== | ==== Project Structure ==== | ||
+ | {{ : | ||
+ | |||
+ | The project is structured in 3 layers: | ||
+ | * Hardware layer - ADXL372 | ||
+ | * Communication layer | ||
+ | * Application layer - ADuCM3029 and EM9304 BLE | ||
- | FIXME! | + | The ADXL372 transmits data to ADuCM3029 controller through |
// End of Document // | // End of Document // |