This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adt7420 [19 Jul 2017 22:17] – launch directions Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_adt7420 [14 Mar 2021 06:04] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== General Description/ | ===== General Description/ | ||
- | The **ADICUP3029_ADT7420** project uses [[http:// | + | The **ADICUP3029_ADT7420** project uses [[adi>en/ |
+ | |||
+ | ===== Demo Video ===== | ||
+ | |||
+ | {{analogTV> | ||
===== Demo Requirements | ===== Demo Requirements | ||
Line 116: | Line 120: | ||
\\ | \\ | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging and Dropping the .Hex to the Daplink drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. | ||
+ | |||
+ | Importing | ||
Line 124: | Line 134: | ||
- | The source code and include files of the **ADICUP3029_ADT7420** demo can be found here: | + | The software for the **ADuCM3029_demo_adt7420** demo can be found here: |
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[https:// | + | Prebuilt ADT7420 Hex File |
+ | * [[https:// | ||
+ | Complete ADT7420 Source Files | ||
+ | * [[https:// | ||
</ | </ | ||
Line 157: | Line 171: | ||
\\ | \\ | ||
\\ | \\ | ||
+ | ====== More Information ====== | ||
+ | |||
+ | {{page> | ||
// End of Document // | // End of Document // | ||