Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [25 Sep 2020 13:47] – [Available commands] Andrei Drimbareanresources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [08 Mar 2021 02:27] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo
Line 79: Line 79:
 {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad71248pmdz_terminal_sample.png |}} {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad71248pmdz_terminal_sample.png |}}
  
-===== Obtaining the Source Code =====+===== Obtaining the Software =====
  
-We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace+There are two basic ways to program the ADICUP3029 with the software for the AD7124-8 PMOD. 
 +  - Dragging and Dropping the .Hex to the Daplink drive 
 +  - Building, Compiling, and Debugging using CCES
  
-The source code and include files of the **ADuCM3029_demo_ad7124_8PMDZ** can be found here:+Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes.  This is the EASIEST way to get started with the reference design
  
-<WRAP round 80% download>+Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain.  
  
-[[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_ad7124_8PMDZ| ADuCM3029_demo_ad7124_8PMDZ at Github]]+The software for the **ADuCM3029_demo_ad7124_8PMDZ** can be found here: 
 + 
 +<WRAP round 80% download> 
 +Prebuilt AD7124-8 PMOD Hex File 
 +  * [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/releases/download/Latest/ADuCM3029_demo_ad7124_8PMDZ.hex| ADuCM3029_demo_ad7124_8PMDZ.Hex]] 
 +Complete AD7124-8 PMOD Source Files 
 +  * [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_ad7124_8PMDZ| ADuCM3029_demo_ad7124_8PMDZ Source Code]]
    
 </WRAP> </WRAP>
resources/eval/user-guides/eval-adicup3029/reference_designs/demo_ad7124-8.1601034468.txt.gz · Last modified: 25 Sep 2020 13:47 by Andrei Drimbarean