Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [11 Aug 2020 16:20] – [Project Structure] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [08 Mar 2021 02:27] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo |
---|
<note important> | |
THIS IS A TEMPLATE.\\ \\ | |
| |
THE GOAL IS TO CREATE A DOCUMENT CUSTOMERS WILL USE WHEN SETTING UP THEIR CFTL DEMO, SO THEY DON'T ASK YOU SO MANY QUESTIONS. IT'S DESIGNED TO HELP YOU GET STARTED WRITING YOUR REFERENCE DEMO USER GUIDE. | |
| |
ALL OF THE CONTENT IS PLACEHOLDER INFORMATION, SO YOU WILL NEED TO POPULATE RELEVANT INFORMATION TO YOUR CFTL. SOME(OR SEVERAL) OF THE SECTION HEADERS MAY NOT APPLY TO YOU, SIMPLY REMOVE THEM. ALSO I MAY NOT HAVE CAPTURED EVERYTHING RELATIVE TO YOUR BOARD, SO ADDING INFORMATION IS ACCEPTABLE. | |
| |
DON'T FORGET TO CREATE A MEDIA FOLDER SPECIFIC TO YOUR DEMO FOR ANY IMAGES, FILES, OR DOCUMENTS YOU WISH TO INCLUDE. THIS WILL HELP US KEEP THE WIKI ORGANIZED AND ENSURE YOUR CONTENT DOESN'T GET REMOVED. | |
</note> | |
| |
====== AD7124-8 PMOD EVAL_ADICUP3029 Demo (w/ EVAL-AD7124-8-PMDZ) ====== | ====== AD7124-8 PMOD EVAL_ADICUP3029 Demo (w/ EVAL-AD7124-8-PMDZ) ====== |
| |
* PC or Laptop with a USB port | * PC or Laptop with a USB port |
* Software | * Software |
* [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_cn0414 | ADuCM3029_demo_ad7124_8PMDZ demo application]] FIXME - LINK | * [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_ad7124_8PMDZ | ADuCM3029_demo_ad7124_8PMDZ demo application]] |
* CrossCore Embedded Studio (2.9.1 or higher) | * CrossCore Embedded Studio (2.9.1 or higher) |
* ADuCM302x DFP (3.2.0 or higher) | * ADuCM302x DFP (3.2.0 or higher) |
===== Setting up the Hardware ===== | ===== Setting up the Hardware ===== |
| |
- Connect **EVAL-AD7124-8-PMDZ** board to the **EVAL-ADICUP3029**. FIXME - PICTURE | - Connect **EVAL-AD7124-8-PMDZ** board to the **EVAL-ADICUP3029**. {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad7124_pmod_unplug.jpg |}} |
- Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. FIXME - PICTURE | - Connect a micro-USB cable to P10 connector of the EVAL-ADICUP3029 and connect it to a computer. The final setup should look similar to the picture below. {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad7124_pmod_plug.jpg |}} |
| |
===== Configuring the Software ===== | ===== Configuring the Software ===== |
| |
The software needs no configuration. FIXME - IIO MENTION IF CASE | The software needs no configuration. |
| |
===== Outputting Data ===== | ===== Outputting Data ===== |
| Register read | //**arr**// | Read an ADC register of a specific address.\\ <//addr//> = Address of the register to be read in hexadecimal base. | **arr 2a** - Read register 0x2A | | | Register read | //**arr**// | Read an ADC register of a specific address.\\ <//addr//> = Address of the register to be read in hexadecimal base. | **arr 2a** - Read register 0x2A | |
| Register write | //**awr**// | Write an ADC register of a specific address with a new value.\\ <//addr//> = Address of the register to be written in hexadecimal base.\\ <//val//> = New value of the register. | **arw 9 8002** - Write 0x8002 to register 0x9. | | | Register write | //**awr**// | Write an ADC register of a specific address with a new value.\\ <//addr//> = Address of the register to be written in hexadecimal base.\\ <//val//> = New value of the register. | **arw 9 8002** - Write 0x8002 to register 0x9. | |
| Get data | //**ags**// | Get a number of samples. Only read the data register the number of times. If the operation takes too long press 'q' to abort.\\ <//no//> = Number of samples (maximum 2048). If sample rate is smaller than 3200 setting the argument 0 means continuous streaming. | | | | Get data | //**ags**// | Get a number of samples per enabled channels. If the operation takes too long press 'q' to abort.\\ <//no//> = Number of samples (maximum 2048). If sample rate is smaller than 3000 setting the argument 0 or no argument means continuous streaming. | | |
| Enable channels | //**aces**// | Choose ADC channels to be activated.\\ <//mask//> = 16-bit mask of the channels to be activated. Can be hexadecimal or binary.\\ A bit of 1 means activated the channel, a bit of 0 means deactivate\\ the channel. | **aces 0xAAAA** - activate every other channel. '0x' is necessary for hexadecimal interpretation. | | | Enable channels | //**aces**// | Choose ADC channels to be activated.\\ <//mask//> = 16-bit mask of the channels to be activated. Can be hexadecimal or binary.\\ A bit of 1 means activated the channel, a bit of 0 means deactivate\\ the channel. | **aces 0xAAAA** - activate every other channel. '0x' is necessary for hexadecimal interpretation. | |
| Get enabled channels | //**aceg**// | Get enable status of ADC channels. Returns a hexadecimal 16-bit mask where bits of 1 represent enabled channels, and bits of 0 represent disabled channels. | | | | Get enabled channels | //**aceg**// | Get enable status of ADC channels. Returns a hexadecimal 16-bit mask where bits of 1 represent enabled channels, and bits of 0 represent disabled channels. | | |
{{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad71248pmdz_terminal_sample.png |}} | {{ :resources:eval:user-guides:eval-adicup3029:reference_designs:ad71248pmdz_terminal_sample.png |}} |
| |
===== Obtaining the Source Code ===== | ===== Obtaining the Software ===== |
| |
We recommend not opening the project directly, but rather import it into CrossCore Embedded Studios and make a local copy in your workspace. | There are two basic ways to program the ADICUP3029 with the software for the AD7124-8 PMOD. |
| - Dragging and Dropping the .Hex to the Daplink drive |
| - Building, Compiling, and Debugging using CCES |
| |
The source code and include files of the **ADuCM3029_demo_ad7124_8PMDZ** can be found here: | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design |
| |
<WRAP round 80% download> | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. |
| |
[[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_cn0414| ADuCM3029_demo_ad7124_8PMDZ at Github]] FIXME - LINK | The software for the **ADuCM3029_demo_ad7124_8PMDZ** can be found here: |
| |
[[| ADuCM3029_demo_ad7124_8PMDZ.HEX]] FIXME - LINK | <WRAP round 80% download> |
| Prebuilt AD7124-8 PMOD Hex File |
| * [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/releases/download/Latest/ADuCM3029_demo_ad7124_8PMDZ.hex| ADuCM3029_demo_ad7124_8PMDZ.Hex]] |
| Complete AD7124-8 PMOD Source Files |
| * [[https://github.com/analogdevicesinc/EVAL-ADICUP3029/tree/master/projects/ADuCM3029_demo_ad7124_8PMDZ| ADuCM3029_demo_ad7124_8PMDZ Source Code]] |
| |
</WRAP> | </WRAP> |