This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [25 Sep 2020 13:47] – [Available commands] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad7124-8 [08 Mar 2021 02:27] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 79: | Line 79: | ||
{{ : | {{ : | ||
- | ===== Obtaining the Source Code ===== | + | ===== Obtaining the Software |
- | We recommend not opening | + | There are two basic ways to program |
+ | - Dragging | ||
+ | - Building, Compiling, and Debugging using CCES | ||
- | The source code and include files of the **ADuCM3029_demo_ad7124_8PMDZ** can be found here: | + | Using the drag and drop method, |
- | <WRAP round 80% download> | + | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download |
- | [[https:// | + | The software for the **ADuCM3029_demo_ad7124_8PMDZ** can be found here: |
+ | |||
+ | <WRAP round 80% download> | ||
+ | Prebuilt AD7124-8 PMOD Hex File | ||
+ | * [[https:// | ||
+ | Complete AD7124-8 PMOD Source Files | ||
+ | * [[https:// | ||
</ | </ |