This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [08 Mar 2021 02:13] – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [08 Mar 2021 02:22] (current) – [Obtaining the Source Code] adding in .Hex files Zuedmar Arceo | ||
---|---|---|---|
Line 82: | Line 82: | ||
===== Obtaining the Software ===== | ===== Obtaining the Software ===== | ||
- | There are two basic ways to program the ADICUP3029 with the software for the AD5992/AD5993. | + | There are two basic ways to program the ADICUP3029 with the software for the AD5592/AD5593 PMOD. |
- Dragging and Dropping the .Hex to the Daplink drive | - Dragging and Dropping the .Hex to the Daplink drive | ||
- Building, Compiling, and Debugging using CCES | - Building, Compiling, and Debugging using CCES | ||
Line 90: | Line 90: | ||
Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
- | The software for the **ADuCM3029_demo_AD5992r_AD5993r** can be found here: | + | The software for the **ADuCM3029_demo_ad5592r_ad5593r** can be found here: |
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | Prebuilt | + | Prebuilt |
- | * [[https:// | + | * [[https:// |
- | Complete | + | Complete |
- | * [[https:// | + | * [[https:// |
</ | </ |