This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [01 Oct 2019 15:34] – [Available commands] Brandon Bushey | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [22 Nov 2019 14:13] – Add treaming command Andrei Drimbarean | ||
---|---|---|---|
Line 70: | Line 70: | ||
^ Mode commands ^ ^ ^ | ^ Mode commands ^ ^ ^ | ||
| //m// | m | Start mirror mode. This mode sets 4 channels as input and 4 channels as output. Then the application reads the input channels and drives the corresponding output channel to the value read on the input channel. For example, if channel 0 reads 1V then the corresponding channel, channel 7, will output 1V. The channels are linked the following way:\\ * Channel 0 (ADC) → Channel 7 (DAC);\\ * Channel 1 (ADC) → Channel 6 (DAC);\\ * Channel 2 (input GPIO) → Channel 5 (output GPIO);\\ * Channel 3 (input GPIO) → Channel 4 (output GPIO). | | | //m// | m | Start mirror mode. This mode sets 4 channels as input and 4 channels as output. Then the application reads the input channels and drives the corresponding output channel to the value read on the input channel. For example, if channel 0 reads 1V then the corresponding channel, channel 7, will output 1V. The channels are linked the following way:\\ * Channel 0 (ADC) → Channel 7 (DAC);\\ * Channel 1 (ADC) → Channel 6 (DAC);\\ * Channel 2 (input GPIO) → Channel 5 (output GPIO);\\ * Channel 3 (input GPIO) → Channel 4 (output GPIO). | | ||
- | | //t// | t | Start production test mode. The following connections must be made:\\ * Channel 0 → Channel 7;\\ * Channel 1 → Channel 6;\\ * Channel 2 → Channel 5;\\ * Channel 3 → Channel 4.\\ Test mode sets CH0:3 to DAC mode, CH4:7 to ADC mode. CH0:3 are set to 0.5V, 1V, 1.5V, 2V, and the voltages at CH4:7 are read back and compared to the expected value. A pass message is then displayed if all the values are read back correctly. | | + | | //t// | t | Start production test mode. The following connections must be made:\\ * Channel 0 → Channel 7;\\ * Channel 1 → Channel 6;\\ * Channel 2 → Channel 5;\\ * Channel 3 → Channel 4.\\ Test mode sets CH0:3 to DAC mode, CH4:7 to ADC mode. CH0:3 are set to 0.5V, 1V, 1.5V, 2V, and the voltages at CH4:7 are read back and compared to the expected value. A pass message is then displayed if all the values are read back correctly. | |
+ | | //ais// <// | ||
* For the " | * For the " |