Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [01 Oct 2019 08:39] – [Available commands] Andrei Drimbarean | resources:eval:user-guides:eval-adicup3029:reference_designs:demo_ad5592r_ad5593r [22 Nov 2019 14:13] – Add treaming command Andrei Drimbarean |
---|
| //di// <//chan//> | di 5 | Change the channel to digital input and read it's state.\\ <//chan//> = channel to be changed and read. (0-7). | | | //di// <//chan//> | di 5 | Change the channel to digital input and read it's state.\\ <//chan//> = channel to be changed and read. (0-7). | |
^ Mode commands ^ ^ ^ | ^ Mode commands ^ ^ ^ |
| //m// | m | Start mirror more. This mode sets 4 channels as input and 4 channels as output. Then the application reads the input channels and drives the corresponding output channel to the value read on the input channel. For example, if channel 0 reads 1V then the corresponding channel, channel 7, will output 1V. The channels are linked the following way:\\ * Channel 0 (ADC) → Channel 7 (DAC);\\ * Channel 1 (ADC) → Channel 6 (DAC);\\ * Channel 2 (input GPIO) → Channel 5 (output GPIO);\\ * Channel 3 (input GPIO) → Channel 4 (output GPIO). | | | //m// | m | Start mirror mode. This mode sets 4 channels as input and 4 channels as output. Then the application reads the input channels and drives the corresponding output channel to the value read on the input channel. For example, if channel 0 reads 1V then the corresponding channel, channel 7, will output 1V. The channels are linked the following way:\\ * Channel 0 (ADC) → Channel 7 (DAC);\\ * Channel 1 (ADC) → Channel 6 (DAC);\\ * Channel 2 (input GPIO) → Channel 5 (output GPIO);\\ * Channel 3 (input GPIO) → Channel 4 (output GPIO). | |
| //t// | t | Start production test mode. The following connections must be made:\\ * Channel 0 → Channel 7;\\ * Channel 1 → Channel 6;\\ * Channel 2 → Channel 5;\\ * Channel 3 → Channel 4.\\ Test mode sets CH0:3 to DAC mode, CH4:7 to ADC mode. CH0:3 are set to 0.5V, 1V, 1.5V, 2V, and the voltages at CH4:7 are read back and compared to the expected value. A pass message is then displayed if all the values are read back correctly. | | | //t// | t | Start production test mode. The following connections must be made:\\ * Channel 0 → Channel 7;\\ * Channel 1 → Channel 6;\\ * Channel 2 → Channel 5;\\ * Channel 3 → Channel 4.\\ Test mode sets CH0:3 to DAC mode, CH4:7 to ADC mode. CH0:3 are set to 0.5V, 1V, 1.5V, 2V, and the voltages at CH4:7 are read back and compared to the expected value. A pass message is then displayed if all the values are read back correctly. | |
| | //ais// <//ch_no//> | ais a | Start streaming mode. This mode reads the selected ADC channel twice a second and outputs the data to the terminal. \\ <//chan//> = channel to be read (0-7) or all channels simultaneously (a). \\ If the channel picked is not an ADC channel the terminal will show an appropriate message. \\ This command does not change the setting of the channels. The desired channels need to be set as ADC separately. | |
| |
* For the "h", "stts", "m" and "t" commands press Enter without inserting any space afterwards. | * For the "h", "stts", "m" and "t" commands press Enter without inserting any space afterwards. |