This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:hardware:cn0418 [02 May 2019 09:30] – Jardine Peñaflor | resources:eval:user-guides:eval-adicup3029:hardware:cn0418 [29 Jul 2021 05:36] (current) – [Registration] Zuedmar Arceo | ||
---|---|---|---|
Line 10: | Line 10: | ||
- | This user guide will discuss how to use the [[http:// | + | This user guide will discuss how to use the [[adi>EVAL-ADICUP3029|EVAL-EVAL-ADICUP3029]] and evaluation software to configure and collect data from the [[adi>CN0418|EVAL-CN0418-ARDZ Evaluation Board]] **(CN-0418 Board)**. |
- | {{ : | + | {{ : |
- | =====EVAL-CN0418-ARDZ attached to EVAL-ADICUP3029===== | + | ======EVAL-CN0418-ARDZ attached to EVAL-ADICUP3029====== |
Line 27: | Line 27: | ||
- | ===== Simplified functional block diagram ===== | + | ====== Simplified functional block diagram |
- | {{ : | + | {{ : |
\\ | \\ | ||
- | ===== Equipment ===== | ||
- | | + | |
- | * [[http:// | + | ===== General Setup ===== |
+ | ==== Equipment ==== | ||
+ | |||
+ | | ||
+ | * [[adi>EVAL-ADICUP3029|EVAL-ADICUP3029 Base Board]] | ||
* PC with a USB port and Windows 7 (32-bit) or higher | * PC with a USB port and Windows 7 (32-bit) or higher | ||
* Serial Terminal Software (Putty/ | * Serial Terminal Software (Putty/ | ||
Line 42: | Line 45: | ||
* USB type A to micro USB type A cable | * USB type A to micro USB type A cable | ||
* CN0418 Evaluation Software | * CN0418 Evaluation Software | ||
- | |||
- | ===== General Setup ===== | ||
{{: | {{: | ||
- | * The [[http:// | + | * The [[adi>CN0418|EVAL-CN0418-ARDZ]] **(CN-0418 Board)** connects to the [[adi>EVAL-ADICUP3029|EVAL-ADICUP3029]] **(ADICUP3029 Board)** |
- | * The [[http:// | + | * The [[adi>EVAL-ADICUP3029|EVAL-ADICUP3029]] **(ADICUP3029 Board)** connects to the PC via the USB cable. |
* Terminal block **P1** is the power supply input (input:+24V DC) | * Terminal block **P1** is the power supply input (input:+24V DC) | ||
* Terminal blocks **P6** provide the quad channel voltage output (-10V to +10V), and Current output (0mA to 24mA) and standard 4 mA to 20 mA HART compatible current inputs. | * Terminal blocks **P6** provide the quad channel voltage output (-10V to +10V), and Current output (0mA to 24mA) and standard 4 mA to 20 mA HART compatible current inputs. | ||
- | ===== Power Supply Considerations and Configuration (P17) ===== | + | ==== Power Supply Considerations and Configuration (P1) ==== |
Terminal block **P17** is the power supply input (input range:+12V to +36V DC). The EARTH terminal can be connected to an external earth connection, to the GND terminal or left floating if an external earth connection is not used. The Green power LED should lit up when connected to a power supply. | Terminal block **P17** is the power supply input (input range:+12V to +36V DC). The EARTH terminal can be connected to an external earth connection, to the GND terminal or left floating if an external earth connection is not used. The Green power LED should lit up when connected to a power supply. | ||
Line 60: | Line 61: | ||
- | ===== Default Shunt Jumper (P9 and P10) and DIP Switches (S3 and S4) Configuration | + | ==== Default Shunt Jumper (P9 and P10) and DIP Switches (S3 and S4) Configuration ==== |
The default jumper position for **P9** and **P10** are shorted at position 1 and 2 while the two DIP switches **S3** and **S4** should be in **ON state** switch position. | The default jumper position for **P9** and **P10** are shorted at position 1 and 2 while the two DIP switches **S3** and **S4** should be in **ON state** switch position. | ||
{{ : | {{ : | ||
- | |||
- | ===== Default EEPROM Address configuration of Solder Jumper position JP2, JP3 and JP4 ===== | ||
- | EEPROM default address configuration of the board is " | ||
- | |||
- | {{ : | ||
- | |||
- | |||
- | |||
- | ===== Default EEPROM WP ( Write Protect) mode configuration of Solder Jumper JP1 ==== | ||
- | EEPROM **WP** pin can be configured as single or multi board operation. The default connection of **WP** pin is shorted to GND. | ||
- | |||
- | {{ : | ||
- | ===== 16 bit Voltage and Current Analog Output Connection (P6) ===== | ||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
^ P9 jumper connections for HART enable (EN) control ^^^ P10 jumper connections for Chip select (SYNC) control ^^^ | ^ P9 jumper connections for HART enable (EN) control ^^^ P10 jumper connections for Chip select (SYNC) control ^^^ | ||
===Single board=== | ===Single board=== | ||
Line 99: | Line 77: | ||
| pin 8 & pin 6 {{: | | pin 8 & pin 6 {{: | ||
+ | ==== Default EEPROM Address configuration of Solder Jumper position JP2, JP3 and JP4 ==== | ||
+ | EEPROM default address configuration of the board is " | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | |||
+ | ==== Default EEPROM WP ( Write Protect) mode configuration of Solder Jumper JP1 ==== | ||
+ | EEPROM **WP** pin can be configured as single or multi board operation. The default connection of **WP** pin is shorted to GND. | ||
+ | |||
+ | {{ : | ||
^ JP1 soldering position ^^ | ^ JP1 soldering position ^^ | ||
^ Position ^ Description ^ | ^ Position ^ Description ^ | ||
Line 104: | Line 93: | ||
| pin 2 & pin 1 {{ : | | pin 2 & pin 1 {{ : | ||
- | + | ==== 16 bit Voltage and Current Analog Output Connection (P6) ==== | |
+ | {{ : | ||
+ | |||
- | ===== Peripheral Connectors | + | ====Peripheral Connectors ==== |
- | All connector pinouts for the EVAL-CN0414-ARDZ are described in the table below. | + | All connector pinouts for the EVAL-CN0418-ARDZ are described in the table below. |
^ Connector | ^ Connector | ||
Line 150: | Line 142: | ||
Up to four EVAL-CN0418-ARDZ boards can be controlled by a single Arduino or EVAL-ADICUP3029 base board by using a simple control scheme. This control scheme will control the SYNC, CD and RX signals to avoid a data conflict. | Up to four EVAL-CN0418-ARDZ boards can be controlled by a single Arduino or EVAL-ADICUP3029 base board by using a simple control scheme. This control scheme will control the SYNC, CD and RX signals to avoid a data conflict. | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
- | * [[https:// | + | * [[https:// |
* [[ADI> | * [[ADI> | ||
* [[ADI> | * [[ADI> | ||
Line 172: | Line 164: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[http:// | + | [[adi>cn0418-designsupport|EVAL-CN0418-ARDZ Design & Integration Files]] |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
Line 181: | Line 173: | ||
====== Software ====== | ====== Software ====== | ||
* [[resources: | * [[resources: | ||
- | + | ||
+ | =====Registration===== | ||
+ | <WRAP round tip 80% > | ||
+ | Receive software update notifications, | ||
+ | </ | ||
// End of Document // | // End of Document // |