This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-ad8302-ardz [06 May 2020 09:13] – adding links to product page and software Adrian Tolentino | resources:eval:user-guides:eval-ad8302-ardz [06 May 2020 09:55] – Adrian Tolentino | ||
---|---|---|---|
Line 30: | Line 30: | ||
- Set up **EVAL-ADICUP3029 serial driver** as in **[[https:// | - Set up **EVAL-ADICUP3029 serial driver** as in **[[https:// | ||
- Download the software on the [[https:// | - Download the software on the [[https:// | ||
- | - Extract the Software GUI file to your computer. | + | - Extract the Software GUI.zip to your computer. |
- Connect the EVAL-ADICUP3029 board using micro USB cable | - Connect the EVAL-ADICUP3029 board using micro USB cable | ||
- Set the **S2 switch to USB**.\\ {{: | - Set the **S2 switch to USB**.\\ {{: | ||
Line 189: | Line 189: | ||
- Connect the EVAL-ADICUP3029 board using micro USB cable. | - Connect the EVAL-ADICUP3029 board using micro USB cable. | ||
- In the EVAL-ADICUP3029, | - In the EVAL-ADICUP3029, | ||
- | - Extract | + | - Unzip **power detector development code-release.zip** from **[[https:// |
+ | - Find and copy **power_detector-firmware.hex** to the DAPLINK directory. Wait for the window to exit automatically. Else, repeat the [[# | ||
- Press S1 (reset) button on the EVAL-ADICUP3029 and mount the EVAL-AD8302-ARDZ to the EVAL-ADICUP3029 | - Press S1 (reset) button on the EVAL-ADICUP3029 and mount the EVAL-AD8302-ARDZ to the EVAL-ADICUP3029 | ||
- | - On pyCharm, go to File>> | + | - On pyCharm, go to File>> |
- Click Project Tab located at left side of IDE and go to **ad8302** folder and double click **ad8302-getShieldReadings.py** | - Click Project Tab located at left side of IDE and go to **ad8302** folder and double click **ad8302-getShieldReadings.py** | ||
- Change the default Port number (“COM10”) in the example code. On your computer go to Control Panel>> | - Change the default Port number (“COM10”) in the example code. On your computer go to Control Panel>> |