This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [16 Jun 2019 23:23] – Dave A | resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [22 Oct 2019 17:03] (current) – Micheál Lambe | ||
---|---|---|---|
Line 29: | Line 29: | ||
- Set S5 to Wall/USB to power the board from the USB cable{{ : | - Set S5 to Wall/USB to power the board from the USB cable{{ : | ||
- Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**. | - Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**. | ||
- | - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 (to use the USB connected probe with EVAL-AD5940ELCZ, | + | - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 to connect the dummy sensor to the AD5940 |
- | - Place jumper in position B on JP6 to connect the 1kΩ||3kΩ RE0 and SE0 | + | - Place jumper in position B on JP6 to connect the 10kΩ||10kΩ resistor divider between |
- Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | ||
Line 49: | Line 49: | ||
^ Variable Name in Firmware ^Description ^ | ^ Variable Name in Firmware ^Description ^ | ||
^ RampStartVolt| This variable sets the voltage at which the excitation signal begins | ^ RampStartVolt| This variable sets the voltage at which the excitation signal begins | ||
- | ^ RampPeakVolt | This sets the peak voltage of the signal. | + | ^ RampPeakVolt | This sets the peak voltage of the signal. |
- | ^ VzeroStart | + | ^ VzeroStart |
^ VzeroPeak | This sets the start voltage on Vzero. Optimully 1.3V. The Actual peak voltage on the sensor pin is VzeroPeak + RampPeakVolt | ^ VzeroPeak | This sets the start voltage on Vzero. Optimully 1.3V. The Actual peak voltage on the sensor pin is VzeroPeak + RampPeakVolt | ||
^ StepNumber | ^ StepNumber |