This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [08 Jul 2019 17:28] – Micheál Lambe | resources:eval:user-guides:eval-ad5940:software_examples:ad5940_ramp [22 Oct 2019 17:03] (current) – Micheál Lambe | ||
---|---|---|---|
Line 29: | Line 29: | ||
- Set S5 to Wall/USB to power the board from the USB cable{{ : | - Set S5 to Wall/USB to power the board from the USB cable{{ : | ||
- Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**. | - Place the **EVAL-AD5940ELCZ** on top of the **EVAL-ADICUP3029**. | ||
- | - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 (to use the USB connected probe with EVAL-AD5940ELCZ, | + | - Ensure jumper on JP10 and JP11 is on PIN2 and PIN4 to connect the dummy sensor to the AD5940 |
- | - Place jumper in position B on JP6 to connect the 1kΩ||3kΩ RE0 and SE0 | + | - Place jumper in position B on JP6 to connect the 10kΩ||10kΩ resistor divider between |
- Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | - Plug in the micro USB cable into the (P10) USB port on the EVAL-ADICUP3029, | ||