This is an old revision of the document!
This demo will use EVAL-ADICUP3029, EVAL_AD5940BIOZ and Impedance-Test board to carry out BIA measurements.
This example project is designed to carry out body impedance analysis. With the nature of body impedance measurements it is difficult to determine if the measurement is correct. Thus, a the Impedance Test board is provided with the hardware which models body impedance. I consists of a range of resistors and capacitors which can be used to model body impedance, contact impedance and electrode impedance.
Alternatively, the custom cables can be connected to the body to measure actual body impedance.
The following is a list of items needed in order to replicate this demo.
The source code and include files for the project can be found on Git
Add link to Git
To compile and run the example open the project in either Keil or IAR.
The measurement results are sent to the PC via UART. To establish connection over UART, connect the Micro-USB cable to the PC and to the EVAL-ADICUP3029 board. A terminal program such as RealTerm or Putty is required to display the results
Following is the UART configuration.
Select COM Port Baud rate: 230400 Data: 8 bit Parity: none Stop: 1 bit Flow Control: none
End of Document