This is an old revision of the document!
The EVAL-AD5940ELCZ shield was designed specifically for carrying out electrochemical measurements. These include:
The platform is an Arduino form factor that can be used with any Arduino form-factor base board. This section describes the features of the evaluation board and how to use it.
All the connectors and their default configurations are described in the table below.
Connector | Jmpr Position. | Description |
---|---|---|
JP1 (DVDD) | A | DVDD powered from 3.3V on Arduino Header (Default) |
B | DVDD powered from LDO | |
C | DVDD powered from external source connected to P11 | |
JP2 (AVDD) | A | AVDD powered from 3.3V on Arduino Header (Default) |
B | AVDD powered from LDO | |
C | AVDD powered from external source connected to P8 | |
JP3 (Reset) | A | Reset pin connected to ARST Button (Default) |
B | Reset pin connected to Arduino Header Reset pin | |
C | Reset pin connected to Arduino header P1.3 (Default) | |
P9 (LDO Enable) | 1-2 | LDO Enabled |
2-3 | LDO Disabled (Default) | |
P10 (LDO Aux Enable) | 1-2 | LDO Enabled |
2-3 | LDO Disabled (Default) | |
JP6 (Dummy RC) | A | Connect network A to CE, RE and SE (Default) |
B | Connect network B to CE, RE and SE | |
JP9 (DE0 Mux) | A | DE0 connected to Gas sensor connector |
B | DE0 connected to dummy network | |
C | DE0 connected to USB port | |
JP10 (RE0 Mux) | A | RE0 connected to dummy network |
B | RE0 connected to gas sensor | |
C | RE0 connected to USB port | |
JP11 (SE0 Mux) | A | SE0 connected to dummy network |
B | SE0 connected to gas sensor | |
C | SE0 connected to USB port | |
JP4 (Cable Shield Mux) | A | Shield connected to CE0 |
B | Shield connected to Bead | |
JP5 (BNC Mux) | A | Water conductivity |
B | pH Measurement | |
C | Connected to AFE1 |
The USB connector provides an interface to connected the USB to Crocodile cable to the AD5940. This USB connector must NEVER be connected to power. If this happens the the AD5940 may become permanently destroyed.
M1 is an Electrochemical gas sensor socket. Standard EC gas sensors can be connected to perform gas sensor measurements. When measuring a Gas sensor ensure JP9, JP10 and JP11 are switched to position C.
The BNC connector is connected to the AD5940 via LTC6078 amplifier. This amplifier can be used with high impedance sensor's such as pH sensors and for water conductivity measurements.
EVAL-AD5940ELCZ Rev A Design and Integration Files