This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [11 Apr 2019 15:42] – [Schematics, PCB Layout, Bill of Materials] Micheál Lambe | resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [09 Aug 2021 13:43] – [USB Connector] Akila M | ||
---|---|---|---|
Line 29: | Line 29: | ||
| ::: | B| Pull down resistor (R25)connected electrode bias | | | ::: | B| Pull down resistor (R25)connected electrode bias | | ||
^ JP6 (Default DNI) | A| Pull up resistor (R42) connected to electrode bias | ^ JP6 (Default DNI) | A| Pull up resistor (R42) connected to electrode bias | ||
- | | ::: | B| Pull down resistor (R42)connected electrode bias | | + | | ::: | B| Pull down resistor (R42)connected electrode bias | |
- | | ::: | C| DE0 connected to USB port | | + | |
^ JP7 (Bias Select) | 3-1| Electrode bias connected to REFOUTS | ^ JP7 (Bias Select) | 3-1| Electrode bias connected to REFOUTS | ||
| ::: | 3-4| Electrode bias connected RLD | | ::: | 3-4| Electrode bias connected RLD | ||
Line 43: | Line 42: | ||
* The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop | * The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop | ||
* The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches. | * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches. | ||
- | Note, the USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected. | + | Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected. |
+ | |||
+ | ECG Cables: | ||
+ | Red = F+ | ||
+ | Black = F- | ||
+ | Green = S+ | ||
+ | Blue = S- | ||
===== Schematics, PCB Layout, Bill of Materials ===== | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | EVAL-AD5940BIOZ Rev B Schematic | + | EVAL-AD5940BIOZ Rev B Design Files |
* {{ : | * {{ : | ||
* {{ : | * {{ : |