This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [29 Nov 2018 14:48] – Micheál Lambe | resources:eval:user-guides:eval-ad5940:hardware:eval-ad5940bioz [12 Feb 2024 15:43] – [USB Connector] Akila M | ||
---|---|---|---|
Line 29: | Line 29: | ||
| ::: | B| Pull down resistor (R25)connected electrode bias | | | ::: | B| Pull down resistor (R25)connected electrode bias | | ||
^ JP6 (Default DNI) | A| Pull up resistor (R42) connected to electrode bias | ^ JP6 (Default DNI) | A| Pull up resistor (R42) connected to electrode bias | ||
- | | ::: | B| Pull down resistor (R42)connected electrode bias | | + | | ::: | B| Pull down resistor (R42)connected electrode bias | |
- | | ::: | C| DE0 connected to USB port | | + | |
^ JP7 (Bias Select) | 3-1| Electrode bias connected to REFOUTS | ^ JP7 (Bias Select) | 3-1| Electrode bias connected to REFOUTS | ||
| ::: | 3-4| Electrode bias connected RLD | | ::: | 3-4| Electrode bias connected RLD | ||
Line 37: | Line 36: | ||
^ P16 | 1-2| Pull up resistor R46 for ECG_P to electrode bias (Default) | | ^ P16 | 1-2| Pull up resistor R46 for ECG_P to electrode bias (Default) | | ||
| ::: | 2-3| Pull down resistor R46 for ECG_P to GND | | | ::: | 2-3| Pull down resistor R46 for ECG_P to GND | | ||
- | ^ P17 | 1-2| Pull up resistor | + | ^ P17 | 1-2| Pull up resistor |
- | | ::: | 2-3| Pull down resistor | + | | ::: | 2-3| Pull down resistor |
===== USB Connector ===== | ===== USB Connector ===== | ||
+ | The Micro USB connector, P6, on the EVAL-AD5940BIOZ board serves 2 functions. | ||
+ | * The provided ECG cables can be connected to a human body simulator which can be used to verify ECG, body composition etc. Note: The EVAL-AD5940BIOZ must never be connected to the human body while the board is connected to a PC or Laptop | ||
+ | * The provided AD5940 Z Test board can also be connected to the Micro USB connecter. This board contains a number of banks of resistors and capacitors which can be used to model Body Impedance, Skin Impedance, Electrode impedances and Contact impedance. These resistor values are configured with the various switches. | ||
+ | Note, P6 USB connector must only be used with the supplied AD5940 Z Test board or the provided ECG Cables. No other cable should ever be connected. | ||
+ | |||
+ | Micro USB pinout for connecting ECG Cables: | ||
+ | ^USB pin | ||
+ | ^1 | ||
+ | ^2 |S+ (ECG IN+)| | ||
+ | ^3 | ||
+ | ^4 | ||
+ | ^5 | ||
+ | |||
+ | |||
+ | ===== Schematics, PCB Layout, Bill of Materials ===== | ||
+ | <WRAP round 80% download> | ||
+ | |||
+ | EVAL-AD5940BIOZ Rev B Design Files | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | * {{ : | ||
+ | |||
+ | </ | ||
+ | |||