This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:eval-ad4116asdz:hardware_guide [16 Nov 2021 11:37] – created Jellenie Rodriguez | resources:eval:user-guides:eval-ad4116asdz:hardware_guide [17 Dec 2021 07:55] (current) – Andrei Alejandro | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== Hardware Guide ===== | ===== Hardware Guide ===== | ||
==== Device Description ==== | ==== Device Description ==== | ||
- | The AD4116 is a highly accurate, high resolution, multiplexed, | + | The [[adi> |
- | See the AD4116 | + | See the AD4116 |
==== Set-up Procedures ==== | ==== Set-up Procedures ==== | ||
After following the instructions in the Software Installation Procedures section, set up the evaluation board and SDP board as detailed in the Configuring the Evaluation and SDP Boards section. | After following the instructions in the Software Installation Procedures section, set up the evaluation board and SDP board as detailed in the Configuring the Evaluation and SDP Boards section. | ||
- | <WRAP center round alert 60%> | + | <note important> |
- | The evaluation software and drivers must be installed before connecting the EVAL-AD4116ASDZ evaluation board and EVAL-SDP-CB1Z board to the USB port of the PC to ensure the PC correctly recognizes the evaluation system. | + | The evaluation software and drivers must be installed before connecting the EVAL-AD4116ASDZ evaluation board and EVAL-SDP-CB1Z board to the USB port of the PC to ensure the PC correctly recognizes the evaluation system. |
- | </WRAP> | + | </note> |
**Configuring the Evaluation and SDP Boards**\\ | **Configuring the Evaluation and SDP Boards**\\ | ||
Line 23: | Line 23: | ||
==== Hardware Link Options ==== | ==== Hardware Link Options ==== | ||
^ Link Number | ^ Link Number | ||
- | | LK1 | Inserted | + | | LK1 | Inserted |
| LK2 | Inserted | | LK2 | Inserted | ||
| LK3 | B (USB) | Selects the power supply voltage. **Position A:** board is powered from the external dc power supply connector, J4. **Position B:** board is powered from USB through the SDP or Arduino connector.| | | LK3 | B (USB) | Selects the power supply voltage. **Position A:** board is powered from the external dc power supply connector, J4. **Position B:** board is powered from USB through the SDP or Arduino connector.| | ||
Line 38: | Line 38: | ||
|P1, P2, P3| Voltage inputs to AD4116| Connector, header, 90°, 5 position, 3.81 mm | | |P1, P2, P3| Voltage inputs to AD4116| Connector, header, 90°, 5 position, 3.81 mm | | ||
|P4| Low-level inputs to AD4116 | Connector, header, 90°, 5 position, 3.81 mm | | |P4| Low-level inputs to AD4116 | Connector, header, 90°, 5 position, 3.81 mm | | ||
- | |J4| External supply voltage (optional) | Power socket block, 3-way, 3.81 mm pitch | | + | |J4| External supply voltage (optional) | Power socket block, 3-way, 3.81 mm pitch | |
- | |5| AIN4, TC+ | | + | |J7| Arduino Headers (Power) |
- | |6| AIN5, TC- | | + | |J8| Arduino Header (Analog) |
- | |7| REFIN1+ | | + | |J9| Arduino Header (Digital 1 | 10 Position Receptacle |
- | |8| REFIN1- | | + | |J10| Arduino Header (Digital 0) |
- | ==== Connector | + | |J11| Arduino Header (IFCSP) |
- | ^ Connector | + | |J12| SDP Connector | 120-way connector, |
- | |1| GND/ | + | |J13| Earth for electromagnetic discharge (ESD testing) | Not applicable |
- | |2| Power Switch, Excitation-| | + | |
- | |3| REFIN-/ SENSE- | | + | |
- | |4| AIN6, AINN | | + | |
- | |5| AIN5, AINP | | + | |
- | |6| REFIN+/ SENSE+ | | + | |
- | |7| AVDD, Excitation+ | + | |
- | |8| GND/SHIELD| | + | |
- | ==== Connector | + | |
- | {{: | + | |
- | ==== Connector J4: AIN8-AIN15 connection ==== | + | |
- | ^ Connector | + | |
- | |1| AIN8| | + | |
- | |2| AIN9| | + | |
- | |3| AIN10| | + | |
- | |4| AIN11 | | + | |
- | |5| AIN12 | | + | |
- | |6| AIN13 | | + | |
- | |7| AIN14 | | + | |
- | |8| AIN15| | + | |
- | ==== Connector | + | |
- | ^ Connector | + | |
- | |J5| Optional external connector for a -1.8V supply, allowing external bench top or alternative supply for AVSS when using a split supply to power AD7124| | + | |
- | |J6| Optional external | + | |
- | |J9|Optional external connector, allowing external bench top or alternative supply | + | |
- | ==== Connector J7: ==== | ||
- | ^ Connector | ||
- | |1|IOVDD| | ||
- | |2|GND| | ||
- | |3|AVSS| | ||
- | |3|AVDD| | ||
- | ==== Connector J8 SMB: ==== | ||
- | Straight PCB mount SMB/SMA jack for master clock (not inserted). The EVAL board has the footprint to include an SMA/SMB connector, if using an external clock source to provide the master clock to the ADC. | ||
- | |||
- | ==== Connector J11 PMOD (DNI): | ||
- | {{ : | ||
- | |||
- | {{ : | ||
===== Power Supplies ===== | ===== Power Supplies ===== | ||
- | The evaluation board receives power through | + | By default, |
- | * Linear regulators generate | + | The [[adi> |
- | * Each supply | + | |
- | ==== AVDD==== | ||
- | - **3.3V** supplied by ADP1720-3.3 (LK15, Pos A)(LK18, Pos A) | ||
- | - **1.8V**, split supply supplied by ADP1720-1.8 (LK15, Pos A)(LK18, Pos B) | ||
- | - EXT AVDD (LK15, Pos B). Connector J7 | ||
- | |||
- | ^Supply^Regulator ^ | ||
- | | 3.3V regulator| [[adi> | ||
- | | 1.8V regulator| [[adi> | ||
- | ==== AVSS==== | ||
- | - AVSS shorted to GND via LK31/32/33 (LK17, Pos B) | ||
- | - **-1.8V**, split supply supplied from external connector J7. (LK17, Pos A) | ||
- | |||
- | ==== IOVDD==== | ||
- | - **3.3V**, supplied by ADP150ACBZ-3.3 (LK19, Pos B) | ||
- | - EXT IOVDD (LK19, Pos B) | ||
- | |||
- | |||
- | ^Supply^Regulator ^ | ||
- | | 3.3V regulator| [[adi> | ||
===== Serial Interface ===== | ===== Serial Interface ===== | ||
The evaluation board connects via the serial peripheral interface (SPI) to the Blackfin® [[adi> | The evaluation board connects via the serial peripheral interface (SPI) to the Blackfin® [[adi> | ||
There are four primary signals: CS, SCLK, DIN, and DOUT/RDY (all are inputs, except for DOUT/RDY, which is an output). | There are four primary signals: CS, SCLK, DIN, and DOUT/RDY (all are inputs, except for DOUT/RDY, which is an output). | ||
- | To operate the evaluation board in standalone mode, the AD7124 serial interface lines can be disconnected from the 120-pin header by removing the links LK21-24. The pins from these links can then be used to fly-wire | + | The EVAL-AD4116ASDZ evaluation board connects to any microcontroller board that uses the Arduino standard headers. This can be developed user code in for a variety of platforms. |
+ | |||
+ | To operate the evaluation board in standalone mode, disconnect any board connected, J9 can be used to access all SPI signals and set the input/ | ||
For an introduction to the Serial Peripheral Interface (SPI), click [[adi> | For an introduction to the Serial Peripheral Interface (SPI), click [[adi> | ||
- | {{ : | + | {{ : |
+ | ===== Analog Inputs ===== | ||
+ | Eleven voltage inputs are available on P1 to P3. | ||
+ | If a different common voltage must be set for single-ended measurement, | ||
+ | Five additional low-level inputs are available on P4. The differential voltage for these inputs is ±VREF only. | ||
===== Reference Options ===== | ===== Reference Options ===== | ||
- | The EVAL-AD7124-8SDZ | + | The EVAL-AD4116ASDZ |
- | The reference used for a conversion is selected by choosing the reference | + | Remove LK1 if using a different single-ended external |
+ | In the evaluation software, click the blue pop-up button | ||
- | {{ : | ||
- | Figure 1: Reference Menu from Eval+ Software. | ||
- | {{ : | + | ===== Schematic, PCB Layout, Bill of Materials ===== |
- | Figure 2: Enabling the 2.5V Reference through pop-ups. | + | |
+ | <WRAP center round download 80%> | ||
+ | EVAL-AD4116ASDZ Rev B Design and Integration Files | ||
- | ===== Schematics ===== | + | * {{ : |
- | + | ||
- | <WRAP center round download 60%> | + | |
- | {{ : | + | |
- | </ | + | |
+ | * {{ : | ||
- | ===== Bill of Materials ===== | + | * {{ : |
- | <WRAP center round download 60%> | + | |
- | {{ : | + | |
</ | </ | ||
Line 145: | Line 89: | ||
- | [[resources: | + | [[resources: |
- | [[resources: | + | [[resources: |