This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ev-dng-rfmod-9001z [25 Sep 2018 13:10] – [Design files] Sharath Rao | resources:eval:user-guides:ev-dng-rfmod-9001z [25 Sep 2018 14:02] – [Introduction] Sharath Rao | ||
---|---|---|---|
Line 3: | Line 3: | ||
====Introduction==== | ====Introduction==== | ||
EV-DNG-RFMOD-9001Z provides an easy interface between the RF module (Lexiwave module which contains ADuCM3029 and ADF7023) and the PC, enabling the user to readily access all the peripherals and GPIOs on the RF module. The RF module can either be soldered down to the EV-DNG-RFMOD-9001Z USB Dongle through the castellations or it can be connected through hirose connector. A variety of modules like Lexiwave, Tessera, SG6T and Smartmesh modules can be connected through hirose as the standard pin layout is maintained for all the RF modules in COG ecosystem. The rapid 6LoWPAN module (Lexiwave module) is currently soldered down to the Dongle. | EV-DNG-RFMOD-9001Z provides an easy interface between the RF module (Lexiwave module which contains ADuCM3029 and ADF7023) and the PC, enabling the user to readily access all the peripherals and GPIOs on the RF module. The RF module can either be soldered down to the EV-DNG-RFMOD-9001Z USB Dongle through the castellations or it can be connected through hirose connector. A variety of modules like Lexiwave, Tessera, SG6T and Smartmesh modules can be connected through hirose as the standard pin layout is maintained for all the RF modules in COG ecosystem. The rapid 6LoWPAN module (Lexiwave module) is currently soldered down to the Dongle. | ||
+ | |||
+ | ====Hardware==== | ||
+ | {{: | ||
====High level block diagram==== | ====High level block diagram==== | ||
Line 35: | Line 38: | ||
- TP5 : Pin 20 | - TP5 : Pin 20 | ||
- | ====Design files==== | + | |
- | EV-DNG-RFMOD-9001Z schematics: | + | |
- | EV-DNG-RFMOD-9001Z layout and BOM:{{ : | + | |
- | EV-DNK-RFMOD-9001Z assembly:{{ : | + | |
- | HLM project link: | + | |
===== EV-DNG-RFMOD-9001Z Design and Integration Files ===== | ===== EV-DNG-RFMOD-9001Z Design and Integration Files ===== |