Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:ev-cog-adf7023-9z [25 Sep 2018 12:53] – [Interface] Pranit Jadhav | resources:eval:user-guides:ev-cog-adf7023-9z [25 Sep 2018 13:31] – [Schematics, PCB Layout, Bill of Material] Pranit Jadhav |
---|
====== EV-COG-ADF7023-9Z User Guide ====== | ====== EV-COG-ADF7023-9Z User Guide ====== |
EV-COG-ADF7023-9Z is an evaluation board to evaluate the ADF7023-J High Performance, Low Power, ISM Band FSK/GFSK/MSK/GMSK transceiver IC. The EV-COG-AD3029LZ evaluation board is a motherboard that controls ADF7023-J daughter boards. The daughter board plugs directly into the motherboard to provide a full ADF7023-J development kit for a wide range of applications depending upon the daughterboard selection. The various available daughter boards can be selected from the following Table 1. | **EV-COG-ADF7023-9Z** is an evaluation board to evaluate the **[[adi>ADF7023-J]]** High Performance, Low Power, 902-958MHz ISM Band FSK/GFSK/MSK/GMSK transceiver IC. The **EV-COG-AD3029LZ** MCU Cog board controls **[[adi>ADF7023-J]]** daughter boards. The daughter board plugs directly into the MCU Cog to provide a full ADF7023-J development kit for a wide range of applications depending upon the daughterboard selection. |
| |
====== Features ====== | ====== Features ====== |
| |
====== Interface ====== | ====== Interface ====== |
EV-COG-ADF7023-9Z connects to motherboard through a hirose connector available on the daughter board. The motherboard will power up the daughter board, so no other external power supply is required. The daughter board has a testport P2 which can be used to probe logic analyzer to the GPIOs connecting MCU on the motherboard to ADF7023-J. | EV-COG-ADF7023-9Z connects to MCU Cog through a hirose connector available on the daughter board. The MCU Cog will power up the daughter board, so no other external power supply is required. The daughter board has a testport P2 which can be used to probe logic analyzer to the GPIOs connecting MCU Cog to ADF7023-J. |
| ===== Primary Side ===== |
| {{ :resources:eval:user-guides:ev-cog-adf7023-9z:p.png?nolink&600 |}} |
| |
| ===== Secondary Side ===== |
| {{ :resources:eval:user-guides:ev-cog-adf7023-9z:s.png?nolink&600 |}} |
===== Test Port ===== | ===== Test Port ===== |
{{ :resources:eval:user-guides:ev-cog-adf7023-9z:testport.png?nolink |}} | {{ :resources:eval:user-guides:ev-cog-adf7023-9z:testport.png?nolink&300 |}} |
| ====== Schematics, PCB Layout, Bill of Material ====== |
| <WRAP center round download 60%> |
| * {{ :resources:eval:user-guides:ev-cog-adf7023-9z:02-049613-01-a-1.pdf |Schematics}} |
| * {{ :resources:eval:user-guides:ev-cog-adf7023-9z:05-049613-01-a_ant.xlsx |Bill OF Material}} |
| * {{ :resources:eval:user-guides:ev-cog-adf7023-9z:09-049613-01a.zip |Fabrication Files}} |
| * {{ :resources:eval:user-guides:ev-cog-adf7023-9z:01-049613-01a.zip |Assembly Files}} |
| </WRAP> |
| |
| |