Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:user-guides:ev-cog-ad4050w [03 Sep 2018 08:02] – . Gowtham shanmugaraj | resources:eval:user-guides:ev-cog-ad4050w [03 Jan 2021 22:04] (current) – fix links Robin Getz |
---|
====== EV-COG-AD4050WZ Development Kit ====== | ====== EV-COG-AD4050WZ Development Kit ====== |
| |
The **[[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD4050.html|EV-COG-AD4050WZ]]** (referred also as MCU Cog) is a development platform based on the industry leading ultra low power **[[adi>ADuCM4050]]** 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.\\ | The **[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EV-COG-AD4050.html|EV-COG-AD4050WZ]]** (referred also as MCU Cog) is a development platform based on the industry leading ultra low power **[[adi>ADuCM4050]]** 32-bit ARM Cortex™-M4F microcontroller. The platform is designed to be a development and prototyping vehicle to get customer ideas from concept to production with a minimal risk and faster time to market.\\ |
{{ :resources:eval:user-guides:front_image_new.png?nolink&550|}} | {{ :resources:eval:user-guides:front_image_new.png?nolink&550|}} |
Applications using EV-COG-AD4050WZ board can be developed using one of the following toolchains. | Applications using EV-COG-AD4050WZ board can be developed using one of the following toolchains. |