Wiki

This version (03 Sep 2018 08:00) was approved by Gowtham shanmugaraj.

Tools and Driver Details

There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD4050LZ works with EV-COG-AD4050WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.

This chapter provides all the necessary steps to download, install, and setup the software environment from Analog Devices. There is also information on the different USB modes and drivers needed.

It contains two main sections:

  1. CrossCore Embedded Studio Download & Install - Provides all the necessary instructions on how to download and install the CrossCore Embedded Studios software development environment.
    • CrossCore Embedded Studio Quickstart Userguide - Provides information about using the CrossCore Embedded Studios IDE, in particular, the process of importing, building, debugging, and creating user applications for the EV-COG-AD4050LZ.
  2. Driver Installation for On-board Debugger (CMSIS DAP) - Provides detailed information how to load pre-compiled .HEX or .BIN files using the USB drive of the EV-COG-AD4050LZ board.


End Document

Back

resources/eval/user-guides/ev-cog-ad4050w/tools_driver.txt · Last modified: 03 Sep 2018 07:59 by Gowtham shanmugaraj