This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ev-cog-ad4050lz:quickstart [06 Nov 2017 09:50] – Pranit Jadhav | resources:eval:user-guides:ev-cog-ad4050lz:quickstart [06 Nov 2017 12:34] – [IAR Embedded Workbench for ARM] Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== MCU Cog Quick Start Guide [using CCES] ====== | + | ====== MCU Cog Quick Start Guide ====== |
Setting up EV-COG-AD4050LZ is a three step process. | Setting up EV-COG-AD4050LZ is a three step process. | ||
- IDE Setup | - IDE Setup | ||
- Software Packs & Drivers Setup | - Software Packs & Drivers Setup | ||
- Running an Example Project | - Running an Example Project | ||
- | ===== IDE Setup ===== | + | \\ |
- | - Install Cross Core Embedded Studio | + | EV-COG-AD4050LZ |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | - License Installation | + | |
- | - Start CCES and navigate to Help -> Manage Licenses. | + | |
- | - Click New and enter the license key provided with the EV-COG-AD4050LZ | + | |
- | - Follow | + | |
- | ===== Software Packs and Driver Setup ===== | + | ===== CrossCore Embedded Studio |
- | - Download the following packs for EV-COG-AD4050LZ | + | |
- | * [[https:// | + | |
- | * [[http:// | + | |
- | * [[http:// | + | |
- | - Start CrossCore Embedded Studio. | + | |
- | - Go to CMSIS Pack Manager by navigating to Windows -> | + | |
- | - Click Import Existing Packs icon {{: | + | |
- | - Select all the packs and import. This will install the packs. Ignore the warnings seen on the console window. In order to remove these warnings, additional packs needs to be installed which are available in the last section of this page. | + | |
- | - Please refer to this [[https:// | + | |
- | ===== Running an Example Project ===== | + | [[resources: |
- | - Power the MCU Cog using a USB (micro-B) Cable. You should see a red LED and a yellow LED turn on by default. {{ :resources: | + | |
- | - In CCES IDE, click CMSIS Pack Manager icon {{:resources: | + | |
- | - Select EV-COG-AD4050LZ from the Boards tab on the Left panel. (see below image) | + | |
- | - Copy button_press example from the Examples tab on the Right panel. {{ : | + | |
- | - Click C/C++ perspective icon {{: | + | |
- | - Under Project Explorer select button_press example, click build icon {{: | + | |
- | - Click on Debug icon {{: | + | |
- | - Click " | + | |
- | - Click run {{: | + | |
- | - Now press BTN1 or BTN2 on EV-COG-AD4050LZ | + | |
- | You are all set! | + | ===== IAR Embedded Workbench for ARM ===== |
- | ===== IAR ===== | + | [[resources: |
- | + | \\ | |
- | [[resources: | + | \\ |
- | \\ End Document | + | |
**[[resources: | **[[resources: | ||
+ | |||
+ | \\ End Document \\ |