This is an old revision of the document!
Using Keil IDE with EV-COG-AD3029WZ
There are no seperate toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029WZ, the toolchain,On-Board Peripheral Drivers & Software for EV-COG-AD3029LZ works with EV-COG-AD3029WZ.The user needs to change only the pin muxing based on the application.For help regarding pinmapping refer to the Hardware Details section.
This will be a paragraph talk about why you might want to use Keil with the EV-COG-AD3029LZ.
How to use EV-COG-AD3029WZ with Keil
In order to use EV-COG-AD3029WZ board with Keil, you will need to replicate the following steps.
Install mBed windows serial driver from
-
Open any example-workspace and project from the ADuCM3029 BSP(board support package). I used the SysTick example in the below images
In the Keil toolbar select
Project →
Options →
Debug, and select the “CMSIS DAP” option
Under the CMSIS DAP Settings, select the SW option
Push Crtl+F5 or in the Keil toolbar select Debug → Start/Stop Debug Session
That’s it – You are ready to go.
End of Document
Back