This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ev-cog-ad3029lz [13 Feb 2018 08:28] – correction Pranit Jadhav | resources:eval:user-guides:ev-cog-ad3029lz [03 Jan 2021 21:46] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== EV-COG-AD3029LZ Development Kit ====== | ====== EV-COG-AD3029LZ Development Kit ====== | ||
- | The **[[http:// | + | The **[[adi>en/ |
{{ : | {{ : | ||
Add-on hardware modules (also called as GEARs), MCU drivers and software application examples form Cog ecosystem. This ecosystem helps customers realize the solution faster, and thus helping them in faster time to market products.\\ | Add-on hardware modules (also called as GEARs), MCU drivers and software application examples form Cog ecosystem. This ecosystem helps customers realize the solution faster, and thus helping them in faster time to market products.\\ | ||
Applications using EV-COG-AD3029LZ board can be developed using one of the following toolchains. | Applications using EV-COG-AD3029LZ board can be developed using one of the following toolchains. | ||
- | - CrossCore Embedded Studio 2.6.0 and above - an Eclipse based Analog Devices Interactive Development Environment. | + | - CrossCore Embedded Studio 2.7.0 and above - an Eclipse based Analog Devices Interactive Development Environment. |
- IAR Embedded Workbench for ARM 8.20 and above | - IAR Embedded Workbench for ARM 8.20 and above | ||
- Keil uVision 4 and above | - Keil uVision 4 and above |