This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guides:ev-cog-ad3029lz:tools:other_ide [28 Aug 2017 11:49] – Sumanth Karanth | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Using Keil IDE with EV-COG-AD3029LZ ====== | ||
+ | This will be a paragraph talk about why you might want to use Keil with the ADICUP3029. | ||
+ | |||
+ | ===== How to use EV-COG-AD3029LZ with Keil ===== | ||
+ | In order to use EV-COG-AD3029LZ board with IAR, you will need to replicate the following steps. | ||
+ | - Install mBed windows serial driver from | ||
+ | - [[https:// | ||
+ | - Open any example-workspace and project from the ADuCM3029 BSP(board support package). | ||
+ | - In the Keil toolbar select **Project** → **Options** → **Debug**, and select the “CMSIS DAP” option{{ : | ||
+ | - Under the CMSIS DAP Settings, select the SW option{{ : | ||
+ | | ||
+ | - Push Crtl+F5 or in the Keil toolbar select **Debug** → **Start/ | ||
+ | - That’s it – You are ready to go. | ||
+ | |||
+ | |||
+ | |||
+ | // End of Document // | ||
+ | |||
+ | **[[resources: |