This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ev-cog-ad3029lz:tools:cces_guide [04 Sep 2017 10:49] – [How to install or upgrade the ADuCM302x Device Family Pack (DFP) for CCES] Pranit Jadhav | resources:eval:user-guides:ev-cog-ad3029lz:tools:cces_guide [11 Sep 2018 08:18] (current) – . Gowtham shanmugaraj | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Cross Core Embedded Studio Quickstart User Guide for EV-COG-AD3029LZ====== | + | ====== Cross Core Embedded Studio Quickstart User Guide for EV-COG-AD3029WZ====== |
+ | < | ||
This page describes how to use the ADuCM302x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM302x processor. The ADuCM302x MCU integrates an ARM Cortex-M3 processor with various on-chip peripherals within a single package. | This page describes how to use the ADuCM302x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM302x processor. The ADuCM302x MCU integrates an ARM Cortex-M3 processor with various on-chip peripherals within a single package. | ||
Line 5: | Line 6: | ||
< | < | ||
- | This page describes how to install and work with the Analog Devices ADuCM302x DFP to start developing applications for the EV-COG-AD3029LZ. | + | This page describes how to install and work with the Analog Devices ADuCM302x DFP to start developing applications for the EV-COG-AD3029WZ. |
Additional help documentation can be found by opening CCES and selecting "Help Contents" | Additional help documentation can be found by opening CCES and selecting "Help Contents" | ||
This page covers: | This page covers: | ||
- | - How to install | + | - How to install |
- How to create a new project for the ADuCM3029 | - How to create a new project for the ADuCM3029 | ||
- How to add startup code and core components to a new project for the ADuCM3029 | - How to add startup code and core components to a new project for the ADuCM3029 | ||
Line 30: | Line 31: | ||
{{ : | {{ : | ||
- | ===== How to install | + | ===== How to install |
+ | There are two ways to install packs for CCES as follows. | ||
+ | * Toolchain' | ||
+ | * Download to Local Directory | ||
+ | ==== Toolchain' | ||
+ | Follow below instructions to install packs using the CMSIS Pack Manager. | ||
+ | - Go to Windows -> Perspective -> Open Perspective -> Other... | ||
+ | - Select CMSIS Pack Manager and click OK. {{ : | ||
+ | - On the left hand side of the window, under devices tab, expand **Analog Devices**. | ||
+ | - Expand **ADuCM302x Series** | ||
+ | - Select **ADuCM3029** | ||
+ | - On right hand side, under packs tab, click **Install** on respective packs to be installed. | ||
+ | {{ : | ||
+ | This will install the packs in CCES toolchain. | ||
+ | |||
+ | |||
+ | ==== Download to Local Directory | ||
Please download the following packs to your local directory. | Please download the following packs to your local directory. | ||
- [[https:// | - [[https:// | ||
- | - [[http:// | + | - [[resources:eval: |
- | - [[http:// | + | - [[resources:eval:user-guides: |
- | - [[http:// | + | - [[resources:eval:user-guides: |
- | - [[http:// | + | - [[resources:eval:user-guides:ev-cog-ad3029lz: |
After downloading the .pack files, select the Import Packs button in the CMSIS Pack Manager' | After downloading the .pack files, select the Import Packs button in the CMSIS Pack Manager' | ||
- | You will be prompted to accept a license agreement and after agreeing to it, the CMSIS-Pack file will be installed into CrossCore Embedded Studio' | + | You will be prompted to accept a license agreement and after agreeing to it, Pack file will be installed into CrossCore Embedded Studio' |
{{ : | {{ : | ||
- | ==== ADuCM302x | + | ==== ADuCM3029 |
- | + | === EV-COG-AD3029WZ/ | |
- | There are two Board Support Packs (BSP) available: one for the ADuCM302x EZ-Kit and one for the COG-AD3029. These BSPs can be installed in the same way as the Device Family Pack (DFP) via the CMSIS Pack Manager perspective. | + | |
- | + | ||
- | === EV-COG-AD3029LZ | + | |
The EV-COG-AD3029LZ Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the EV-COG-AD3029LZ Evaluation Board and examples for peripherals on the ADcCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP). | The EV-COG-AD3029LZ Board Support Pack (BSP) provides the drivers for off-chip peripherals which are on the EV-COG-AD3029LZ Evaluation Board and examples for peripherals on the ADcCM3029 processor. The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio and the ADuCM302x Device Family Pack (DFP). | ||
Line 58: | Line 72: | ||
==== ADI Sensor Software Pack ==== | ==== ADI Sensor Software Pack ==== | ||
- | The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with EV-COG-AD3029LZ | + | The ADI Sensor Software pack contains various sensor software components and associated examples. The examples in the sensor pack are designed to work with EV-COG-AD3029WZ |
For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf) | For more information on the ADI Sensor Software Pack, please refer to the User's Guide in the Documents folder (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\packs\AnalogDevices\ADI-SensorSoftware\1.0.0\Documents\SensorSoftware_Users_Guide.pdf) |