This is an old revision of the document!
The EV-COG-AD3029LZ software pack provides access to all the necessary on-board peripheral drivers for the EV-COG-AD3029LZ development platform. This software layer is the secondary layer needed when writing applications using this development platform. The EV-COG-AD3029LZ software pack builds on top of what the ADuCm302x software pack provides. The EV-COG-AD3029LZ software pack makes it easier to use the on-board peripherals so creating your application layer is will be easier. Combined with the ADuCM302x and Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD3029LZ development platform.
The drivers and examples in the BSP are designed to work with CrossCore Embedded Studio 2.6.0 ® and the ADuCM302x Device Family Pack 2.0.0.
EV-COG-AD3029LZ software pack contains the following components:
For detailed information regarding the EV-COG-AD3029LZ software pack, please see our complete EV-COG-AD3029LZ software user guide.
ADD LINK HERER EV-COG-AD3029LZ BSP Release Notes
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ platform.
The software pack can be downloaded in several ways.
End of Document