This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:cn0270 [29 May 2014 17:17] – created James Fitzgerald | resources:eval:user-guides:cn0270 [09 Jan 2021 00:39] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CN0270 Software User Guide ====== | ====== CN0270 Software User Guide ====== | ||
+ | ===== Overview ===== | ||
+ | [[adi> | ||
+ | |||
+ | The EVAL-CN0270-EB1Z evaluation board comes with an onboard ADI microcontroller that handles communication between the system and the evaluation software. It also complies with the double PMOD form factor for use with external processors. | ||
+ | |||
+ | This user guide will discuss how to use the evaluation software to configure and control the [[adi> | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Required Equipment ===== | ||
+ | |||
+ | * EVAL-CN0270-EB1Z Evaluation Board | ||
+ | * USB-SWD/ | ||
+ | * [[ftp:// | ||
+ | * DC power supply, 24V recommended (12V to 36V compatible) | ||
+ | * Multi Meter | ||
+ | * USB Type-A plug to USB Mini-B plug cable | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== General Setup ===== | ||
+ | * The board is supplied via terminal block P1, +24VDC is recommended. | ||
+ | * The current loop output is derived from terminal block P3. | ||
+ | * The **USB-SWD/ | ||
+ | * **Link P2** | ||
+ | * OPEN : disconnects the 499-ohm load resistor across current output and GND | ||
+ | * SHORT : connects a 499-ohm load resistor across current output and GND | ||
+ | * **Link PMOD** | ||
+ | * OPEN : control is via onboard processer and J-Link header.Choose this option if you want to connect the board using the J-Link USB and use the [[ftp:// | ||
+ | * SHORT : control is via PMOD headers. Choose option if you want to use the circuit for prototyping or with external processors | ||
+ | * **Link XTAL** | ||
+ | * Towards position 1 : AD5700-1 is clocked using the on-chip oscillator | ||
+ | * Towards position 0 : AD5700-1 is clocked using the 3.6864 MHz crystal | ||
+ | {{: | ||
+ | {{: | ||
+ | |||
+ | |||
+ | ===== Installing the Software ===== | ||
+ | - Extract the file **CN0270 Eval Software.zip** and open the file **setup.exe**.\\ \\ <WRAP left tip round box 60%> | ||
+ | - Click **Next** to view the installation review page\\ {{: | ||
+ | - Click **Next** to start the installation | ||
+ | - Upon completion of the installation of the CN0270 Evaluation Software, the installer for the ADuCM360 and Segger J-Link Drivers will execute.\\ \\ <WRAP left round tip 60%> | ||
+ | NOTE: It is recommended that you close all other applications before clicking “Next”. This will make it possible to update relevant system files without having to reboot your computer. | ||
+ | </ | ||
+ | - Click **I Agree** to accept the software license agreement and initiate the installation | ||
+ | - Select only **ADuCM360** and **Segger J-Link Software** on the options shown\\ \\ <WRAP left round important 60%> | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | |||
+ | ===== Using the Evaluation Software ===== | ||
+ | ==== Software Controls and Indicator Descriptions ==== | ||
+ | === Main Window === | ||
+ | This Window contains the block diagram of the system and gives access to the different controls and indicators.\\ \\ {{: | ||
+ | - **Output Current** | ||
+ | * This control accepts a numerical value and sets the output current accordingly. Entering a value will also update the DAC Code field to the corresponding value. | ||
+ | - **DAC Code** | ||
+ | * This control accepts data in HEX format and sets the output current according to the code. Entering a value will also update the Output Current field to the corresponding value. | ||
+ | - **Test Current** | ||
+ | * This enables/ | ||
+ | - Open AD5420 Configuration window | ||
+ | - Open HART Modem window | ||
+ | - **Hart Activity Indicator** | ||
+ | * This indicates when there is data that was received in the HART interface. The data may be viewed in the HART Modem window. | ||
+ | - **Reset** | ||
+ | * Resets both the system and evaluation software back to default working settings | ||
+ | - **Status Bar** | ||
+ | * This indicator displays a message to the user detailing the current state of the software. | ||
+ | |||
+ | |||
+ | ---- | ||
+ | |||
+ | === AD5420 Configuration Window === | ||
+ | This window allows for configuration of current output section of the circuit. This window must be closed to resume operation of the software.\\ \\ {{: | ||
+ | - **Output Enabled** | ||
+ | * Unordered List ItemThis triggers the output enabled operation when clicked. | ||
+ | - **Output Range** | ||
+ | * This drop menu configure the output range of the AD5420 by selecting the desired output shown in the menu. | ||
+ | - **Digital Slew Rate Control** | ||
+ | - Enable Button - Enables/ | ||
+ | - Step Size – defines by how much the output value changes at each update. | ||
+ | - Update Rate – defines the rate at which the digital slew is updated. | ||
+ | - **Configure** | ||
+ | * Applies new configurations and closes the configuration window | ||
+ | - **Cancel** | ||
+ | * Close the configuration window without changes | ||
+ | |||
+ | ---- | ||
+ | |||
+ | === HART Modem Window === | ||
+ | This window holds the controls and displays for transmitting and reading data from the HART interface. This window can run in parallel to the main window.\\ \\ {{: | ||
+ | - Receive Buffer – Displays the received HART Data | ||
+ | - HART Page – This shows the HART data divided into the corresponding packets | ||
+ | - Raw – This shows the all HART data bytes received during the last transmission | ||
+ | - Transmit Buffer – Transmit data that is defined by the user. | ||
+ | - HART Page – this page allows the user to configure the HART packet to be transmitted. The software will automatically format the HART packet from the values entered. | ||
+ | - Copy Data from Rx Buffer – Copies data from the receive buffer to the transmit buffer | ||
+ | - Transmit Data – Transmits HART data based the values entered | ||
+ | - Raw – This page allows the user to define the data to be sent without formatting | ||
+ | |||
+ | ---- | ||
+ | |||
+ | ===== Additional Info===== | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | Microcontroller References | ||
+ | * [[ftp:// | ||
+ | * [[adi> | ||
+ | * [[adi> |