This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:circuits-from-the-lab:pulsar-adc-pmods [23 Oct 2017 21:21] – added the change log, and updated the schematic Brandon Bushey | resources:eval:user-guides:circuits-from-the-lab:pulsar-adc-pmods [14 Dec 2017 23:18] – [Evaluation] amending the setup Brandon Bushey | ||
---|---|---|---|
Line 75: | Line 75: | ||
==== Evaluation ==== | ==== Evaluation ==== | ||
- | Evaluating the PulSAR ADC PMOD boards is very simple. | + | Evaluating the PulSAR ADC PMOD boards is very simple. |
- Plug in the Mini USB cable from a USB port on your PC, to the **J1** of the EVAL-SDP-CB1Z.{{ : | - Plug in the Mini USB cable from a USB port on your PC, to the **J1** of the EVAL-SDP-CB1Z.{{ : | ||
- | | + | |
- | - Next take the EVAL-SDP-CB1Z board and connect **CON A** up to **J4** of the SDP-PMD-IB1Z interposer board. | + | - Ensure that you remove the shunt which is located at **JP1** of the SDP-PMD-IB1Z |
+ | - Next take the EVAL-SDP-CB1Z board and connect **CON A** up to **J4** of the SDP-PMD-IB1Z interposer board. | ||
- Connect the EVAL-CFTL-6V-PWRZ to **J1** barrel jack of the SDP-PMD-IB1Z, | - Connect the EVAL-CFTL-6V-PWRZ to **J1** barrel jack of the SDP-PMD-IB1Z, | ||
- | - Place the shunt across **JP1** of the SDP-PMD-IB1Z, | ||
- Take the PulSAR ADC PMOD board you are using and connect it to **J3** of the SDP-PMD-IB1Z interposer board. This should finish the hardware setup.{{ : | - Take the PulSAR ADC PMOD board you are using and connect it to **J3** of the SDP-PMD-IB1Z interposer board. This should finish the hardware setup.{{ : | ||
+ | - With the power source turn **OFF**, connect your external power supplies (-2.5V, GND, and 7.5V) to the terminal block of your EVAL-AD7xxx-PMDZ board. | ||
+ | - Turn **ON** your external power supplies (-2.5V, GND, and 7.5V) connected in the previous step. | ||
+ | - Place the shunt across **JP1** of the SDP-PMD-IB1Z, | ||
- Check again in the device manager to make sure the //ADI Development Tools// are still displaying. | - Check again in the device manager to make sure the //ADI Development Tools// are still displaying. | ||
- | - Connect your external power supplies (-2.5V, GND, and 7.5V) to the terminal block of your EVAL-AD7xxx-PMDZ board. | ||
- Connect your SMB cable from your signal source to the Vin+ and Vin- connectors of the EVAL-AD7xxx-PMDZ board. | - Connect your SMB cable from your signal source to the Vin+ and Vin- connectors of the EVAL-AD7xxx-PMDZ board. | ||
Line 138: | Line 140: | ||
Rev 0 to Rev A | Rev 0 to Rev A | ||
* Changed CAD tools from PADS to Allegro, so the reference designators have changed | * Changed CAD tools from PADS to Allegro, so the reference designators have changed | ||
- | * Replaced C9 and C10(Rev0) and put in R5 and R7(Rev A) so you can digitally control the PD pin of the ADA4841 ADC Driver amplifiers | + | * Replaced C9 and C10(Rev 0) and put in R5 and R7(Rev A) |
* Added R16 and R17(Rev A) to be able to use more operating modes of the ADC (for example, daisy-chain mode) | * Added R16 and R17(Rev A) to be able to use more operating modes of the ADC (for example, daisy-chain mode) | ||
- | * Removed U5 (ADG1401 on Rev0) and connected the 5V reference directly to the ADC (U3 Rev0) | + | * Removed U5 (ADG1401 on Rev 0) and connected the 5V reference directly to the ADC (U3 Rev 0) |
- | * Removed U8 (ADP7104-3.3 on Rev0) and connected the VIO pin of the ADC to VCC (J4 Rev0) | + | * Removed U8 (ADP7104-3.3 on Rev 0) and connected the VIO pin of the ADC to VCC (J4 Rev 0) |
* Separated out the AGND plane and DGND plane | * Separated out the AGND plane and DGND plane | ||
//End of Document// | //End of Document// |