This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:circuits-from-the-lab:fthr-pmd-intz [31 May 2022 10:29] – [SPI Pmod Connector (P6)] Richmond Eustacio | resources:eval:user-guides:circuits-from-the-lab:fthr-pmd-intz [14 Jul 2023 14:34] (current) – Corrected download link for Design & Integration files. Brent Kowal | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== FTHR-PMD-INTZ Hardware User Guide ====== | + | ====== FTHR-PMD-INTZ |
===== Overview ===== | ===== Overview ===== | ||
- | The [[ADI> | + | The [[ADI> |
This interposer board provides such solution and allows interfacing with up to two Pmod boards via SPI or I2C interface. Furthermore, | This interposer board provides such solution and allows interfacing with up to two Pmod boards via SPI or I2C interface. Furthermore, | ||
+ | {{ : | ||
+ | <wrap center 22%> //< | ||
- | \\ | ||
- | \\ | ||
- | <insert isometric view of board> | ||
- | \\ | ||
<WRAP center round info 60%> | <WRAP center round info 60%> | ||
**__Evaluation Kit Contents: | **__Evaluation Kit Contents: | ||
* [[adi> | * [[adi> | ||
</ | </ | ||
- | \\ | + | |
===== Adapter Board Hardware ===== | ===== Adapter Board Hardware ===== | ||
+ | {{ : | ||
+ | <wrap center 22%> //< | ||
- | <insert photo of feather pmod labeled parts> | ||
==== Power Configuration ==== | ==== Power Configuration ==== | ||
The circuit is powered by the voltage coming from the Maxim Feather headers. | The circuit is powered by the voltage coming from the Maxim Feather headers. | ||
- | <insert photo labelled jumpers> | + | {{ : |
+ | <wrap center 22%> //< | ||
\\ | \\ | ||
The table below lists the power configuration for this interposer board. The default voltage configuration for all is 3V3. | The table below lists the power configuration for this interposer board. The default voltage configuration for all is 3V3. | ||
+ | | **Part** | ||
+ | | P2 | Feather Voltage Selector| | ||
+ | | P4 | I2C PMOD Voltage Selector| | ||
+ | | P5 | SPI PMOD Voltage Selector| | ||
==== SPI Pmod Connector (P6) ==== | ==== SPI Pmod Connector (P6) ==== | ||
Connect Pmod devices that use SPI interface to the left-hand side Pmod connector, as shown below. | Connect Pmod devices that use SPI interface to the left-hand side Pmod connector, as shown below. | ||
- | <insert labelled | + | {{ : |
+ | <wrap center 22%> //< | ||
The table below lists the corresponding pin assignment | The table below lists the corresponding pin assignment | ||
+ | ^ SPI Pmod Connector (P6) Pinout | ||
+ | | **Pin Number** | ||
+ | | 1 | **CS**. SPI Chip select #1 from MAXFTHR to the Pmod device.| | ||
+ | | 2 | **MOSI_GPIO1**. SPI data from MAXFTHR to the Pmod device. | 8 | **SPI_GPIO1**. Reset Signal from MAXFTHR to Pmod device | | ||
+ | | 3 | **MISO**. SPI data from MAXFTHR to the Pmod device. | 9 | **SPI_GPIO2**. SPI Chip select #2 from MAXFTHR to the Pmod device. | | ||
+ | | 4 | **SCLK**. SPI Clock from MAXFTHR to the Pmod device. | 10 | **SPI_GPIO3**. SPI Chip select #3 from MAXFTHR to the Pmod device. | | ||
+ | | 5 | **GND**. Ground | 11 | **GND**. Ground| | ||
+ | | 6 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR (shorted in P5).| 12 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR (shorted in P5). | | ||
+ | === I2C Pmod Connector (P7) === | ||
- | === I²C Pmod Connector (P7) === | + | Pmod devices that use I2C interface should be connected to the right Pmod connector. |
- | Pmod devices that use I²C interface should be connected to the right pmod connector. | + | {{ : |
- | + | <wrap center 22%> //<fc>Figure 5. I2C PMOD Connector</fc>// </wrap> | |
- | <insert labelled I<sup>2</sup>C pin> | + | |
The table below lists the corresponding pin assignment | The table below lists the corresponding pin assignment | ||
\\ | \\ | ||
- | \\ | + | ^ |
- | ^ | + | |
| **Pin Number** | | **Pin Number** | ||
- | | 1 | **I²C_GPIO_0**. Interrupt Signal from the Pmod device to the MAXFTHR.| 7 | **I²C_GPIO_0**. Interrupt Signal from the Pmod device to the MAXFTHR. | | + | | 1 | **I2C_GPIO0**. Interrupt Signal from the Pmod device to the MAXFTHR.| |
- | | 2 | **I²C_GPIO_1**. Reset Signal from the MAXFTHR to the Pmod device. | 8 | **I²C_GPIO_1**. Reset Signal from the MAXFTHR to the Pmod device. | | + | | 2 | **I2C_GPIO1**. Reset Signal from the MAXFTHR to the Pmod device. | 8 | **I2C_GPIO1**. Reset Signal from the MAXFTHR to the Pmod device. | |
- | | 3 | **SCL**. | + | | 3 | **SCL**. |
- | | 4 | **SDA**. | + | | 4 | **SDA**. |
- | | 5 | **GND**. Ground | 11 | **GND**. Ground| | + | | 5 | **GND**. Ground | 11 | **GND**. Ground| |
- | | 6 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR | + | | 6 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR (shorted in P4).| 12 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR (shorted in P4). | |
- | (shorted in P4).| 12 | **VCC**. Connected to 3V3 or VBUS from MAXFTHR | + | |
- | (shorted in P4). | | + | |
\\ | \\ | ||
\\ | \\ | ||
- | ==== Sensor Connector #2 (P?) ==== | ||
- | {{: | ||
- | \\ \\ \\ \\ \\ | ||
- | === Sensor Specific Input Configuration === | ||
- | \\ | + | ====== Schematic, PCB Layout, Bill of Materials |
- | {{: | + | |
- | \\ \\ | + | |
- | \\ \\ | + | |
- | < | + | |
- | \\ | + | |
- | + | ||
- | ==== Sensor Connector #3 (P?) ==== | + | |
- | + | ||
- | The EVAL-CN0398-ARDZ shield board comes with a BNC connector J1 for pH sensors as shown on the image below | + | |
- | \\ | + | |
- | {{: | + | |
- | \\ \\ | + | |
- | The output of the pH sensor is bipolar and gives a maximum signal of ±414 mV at 25°C. The [[adi> | + | |
- | \\ | + | |
- | < | + | |
- | \\ | + | |
- | + | ||
- | ==== LED Indicators ==== | + | |
- | + | ||
- | Does your board have LEDs? If yes what do they indicate? | + | |
- | {{ : | + | |
- | + | ||
- | ==== Switches and Buttons ==== | + | |
- | + | ||
- | Are there any switches or reset buttons, describe them. | + | |
- | + | ||
- | ==== Host processor Connector ==== | + | |
- | FMC, Arduino, RPI, PMOD, SDP, Other | + | |
- | + | ||
- | ==== Other Analog/ | + | |
- | + | ||
- | Your board may be more or less complicated, | + | |
- | + | ||
- | ===== Power Supply Considerations and Configuration (P3) ===== | + | |
- | + | ||
- | Terminal block **P3** is the power supply input (input range:+9.5V to +36V DC). The EARTH terminal can be connected to an external earth connection, to the GND terminal or left floating if an external earth connection is not used. | + | |
- | + | ||
- | ^ Main power setup | + | |
- | | {{ : | + | |
- | + | ||
- | ===== Schematic, PCB Layout, Bill of Materials ===== | + | |
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | [[adi>cn0xxx-designsupport|EVAL-CN0xxx-ARDZ Design & Integration Files]] | + | [[adi>media/ |
* Schematics | * Schematics | ||
* PCB Layout | * PCB Layout | ||
* Bill of Materials | * Bill of Materials | ||
* Allegro Project | * Allegro Project | ||
- | * <ADD other things specific to your project if desired> | + | |
</ | </ | ||
- | ===== Additional Information and Useful Links ===== | + | ====== Additional Information and Useful Links ====== |
- | | + | * [[ADI>FTHR-PMD-INTZ|FTHR-PMD-INTZ |
- | | + | * [[ADI>MAX32630FTHR|MAX32630FTHR |
- | * [[ADI> | + | * [[ADI>MAX32650FTHR|MAX32650FTHR |
- | * [[ADI> | + | * [[ADI>MAX32655FTHR|MAX32655FTHR |
- | * [[ADI>AD5700-1|AD5700-1 | + | * [[ADI>MAX32666FTHR|MAX32666FTHR |
- | * [[ADI>ADUM5411|ADUM5411 | + | * [[ADI>MAX78000FTHR|MAX78000FTHR |
- | * [[ADI>ADUM3151|ADUM3151 | + | |
- | * [[ADI>ADP2441|ADP2441 | + | |
- | * [[ADI>ADG704|ADG704 | + | |
====== Reference Demos & Software ====== | ====== Reference Demos & Software ====== | ||
- | * [[resources: | + | * [[resources: |
- | * [[resources: | + | * [[resources: |
+ | * [[resources:eval: | ||
+ | \\ | ||
+ | \\ | ||
// End of Document // | // End of Document // |